SFFS125 June   2021 SN74HCS74-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the SN74HCS74-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to VCC (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality
B No device damage, but loss of functionality
C No device damage, but performance degradation
D No device damage, no impact to functionality or performance

Figure 4-1 shows the SN74HCS74-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the SN74HCS74-Q1 data sheet.

GUID-7B2146FD-DB98-4805-AE9A-4367DEE7C744-low.gifGUID-20201105-CA0I-R51S-5DRT-TCZRPR5P0NLB-low.gifFigure 4-1 Pin Diagram
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin Number Description of Potential Failure Effect(s) Failure Effect Class
1CLR; 1D; 1CLK; 1PRE; 2PRE; 2CLK; 2D; 2CLR 1; 2; 3; 4; 5; 10; 11; 12; 13 Input pin functionality is defined such as input is LOW – See Device Function Table B
1Q; 1Q; 2Q; 2Q 5; 6; 8; 9

Can cause excessive output current; output will not switch

(For example, if buffer output is shorted to ground and is attempting to drive to VCC).

A
VCC 14 The device is not powered, because short is external to the device. System level damage may occur in this scenario. B
GND 7 Normal operation. D
PAD — Normal operation. D
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin Number Description of Potential Failure Effect(s) Failure Effect Class
1CLR; 1D; 1CLK; 1PRE; 2PRE; 2CLK; 2D; 2CLR 1; 2; 3; 4; 5; 10; 11; 12; 13 The pin is floating, and it can change the output state and cause excessive current to flow from VCC to GND. Refer to the Implications of Slow or Floating CMOS Inputs section in the SN74HCS74-Q1 application note for more information. A
1Q; 1Q; 2Q; 2Q 5; 6; 8; 9 Normal operation. D
VCC 14 The device is not powered. B
GND 7 The device is not powered. B
PAD — Normal operation. D
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Shorted to Description of Potential Failure Effect(s) Failure Effect Class
1CLR; 1D; 1CLK; 1PRE; 2PRE; 2CLK; 2D; 2CLR 1CLR; 1D; 1CLK; 1PRE; 2PRE; 2CLK; 2D; 2CLR Two inputs shorted together will not cause damage unless there is an external bus contention that drives the input (such that VIL<Input Voltage<VIH), in which case excessive supply current to GND may cause damage. System level damage may occur in this scenario. A
1CLR; 1D; 1CLK; 1PRE; 2PRE; 2CLK; 2D; 2CLR 1Q; 1Q; 2Q; 2Q Can cause excessive output current, output will not switch (for example, if inverter input is shorted to output). A
1CLR; 1D; 1CLK; 1PRE; 2PRE; 2CLK; 2D; 2CLR GND See Table 4-2 input response for more information. A
1CLR; 1D; 1CLK; 1PRE; 2PRE; 2CLK; 2D; 2CLR VCC See Table 4-5 input response for more information. A
1Q; 1Q; 2Q; 2Q 1Q; 1Q; 2Q; 2Q Can cause excessive output current, and the output will not switch (for example, if one output is driving to VCC and another output is driving to GND). A
1Q; 1Q; 2Q; 2Q GND See Table 4-2 output response for more information. A
1Q; 1Q; 2Q; 2Q VCC See Table 4-5 output response for more information. A
GND VCC The device is not powered, because short is external to the device. System level damage may occur in this scenario. B
PAD VCC The device is not powered, because short is external to the device. System level damage may occur in this scenario. B
PAD Inputs/Outputs Can cause excessive output current, output will not switch. A
Table 4-5 Pin FMA for Device Pins Short-Circuited to VCC
Pin Name Pin Number Description of Potential Failure Effect(s) Failure Effect Class
1CLR; 1D; 1CLK; 1PRE; 2PRE; 2CLK; 2D; 2CLR 1; 2; 3; 4; 5; 10; 11; 12; 13 The input pin functionality is defined as high input. For example, if the buffer input is VCC, then the output will always be driven high. B
1Q; 1Q; 2Q; 2Q 5; 6; 8; 9 Can cause excessive output current, and the output will not switch (for example, if the buffer output is shorted to VCC and is attempting to drive to GND). A
VCC 14 Normal operation. D
GND 7 The device is not powered, because short is external to the device. System level damage may occur in this scenario. B
PAD — The device is not powered, because short is external to the device. System level damage may occur in this scenario. B