SFFS106 November   2021 SN74LVC2G17-Q1

 

  1.   Trademarks
  2. 1Overview
  3. 2Functional Safety Failure In Time (FIT) Rates
  4. 3Failure Mode Distribution (FMD)
  5. 4Pin Failure Mode Analysis (Pin FMA)

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the SN74LVC2G17-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to VCC (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality
B No device damage, but loss of functionality
C No device damage, but performance degradation
D No device damage, no impact to functionality or performance

Figure 4-1 shows the SN74LVC2G17-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the SN74LVC2G17-Q1 data sheet.

GUID-22F8A81A-EA1F-446A-9822-8A084BD7DA01-low.gif Figure 4-1 Pin Diagram
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
Input 1, 3 Input pin functionality is defined such as input is LOW – see the Device Functional Modes section in the SN74LVC2G17-Q1 Automotive Dual Schmitt-Trigger Buffer data sheet (for example, if buffer input is GND, then the output will always be driven LOW). B
Output 4, 6 Can cause excessive output current and output will not switch (for example, if buffer output is shorted to ground and is attempting to drive to VCC). A
VCC 5 Device will not be powered, because short is external to device; system level damage may occur in this scenario. B
GND 2 Normal operation. D
Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
Input 1, 3 Pin is floating; can change output state and cause excessive current from VCC to GND (See Implications of Slow or Floating CMOS Inputs) A
Output 4, 6 Normal operation. D
VCC 5 Device will not be powered. B
GND 2 Device will not be powered. B
Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
Input 1, 3 Input Two inputs shorted together will not cause damage unless there is an external bus contention that drives the input (such that VIL<Input Voltage<VIH) in which case excessive supply current to GND may cause damage; system level damage may occur in this scenario. A
Input 1, 3 Output Can cause excessive output current and output will not switch (for example, if inverter input is shorted to output). A
Input 1, 3 GND See input response in Table 4-2. A
Input 1, 3 VCC See input response in Table 4-5. A
Output 4, 6 Output Can cause excessive output current, and output will not switch (for example, if one output is driving to VCC and another output is driving to GND). A
Output 4, 6 GND See output response in Table 4-2. A
Output 4, 6 VCC See output response in Table 4-5. A
GND 2 VCC Device will not be powered, because short is external to the device; system level damage may occur in this scenario. B
Table 4-5 Pin FMA for Device Pins Short-Circuited to VCC
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
Input 1, 3 Input pin functionality is defined such as input is HIGH – see the Device Functional Modes section in the SN74LVC2G17-Q1 Automotive Dual Schmitt-Trigger Buffer data sheet (for example, if the buffer input is VCC, then the output will always be driven HIGH) B
Output 4, 6 Can cause excessive output current and the output will not switch (for example, if the buffer output is shorted to VCC and is attempting to drive to GND). A
VCC 5 Normal operation. D
GND 2 Device will not be powered, because short is external to the device; system level damage may occur in this scenario. B