SCPU047 December   2022

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2EVM Setup
  5. 3Power
  6. 4Enabling Pull-up Resistors
  7. 5Enabling Bus Capacitance
  8. 6Board Layout
  9. 7Schematic
  10. 8Bill of Materials
  11. 9Revision History

EVM Setup

Equipment needed to evaluate the TCA39416:

  • Two Channel power supply (If VccA=VccB then 1 channel is sufficent)
  • 4 channel oscilloscope if user wishes to observe the I3C transactions on both sides
    • Male SMA connectors which can attach to J5, J7, J12, J17
  • Microcontroller, processor, or digital analyzer which can send and receive I3C