SCPU043 March   2021

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Features
  3. 2EVM Setup
    1. 2.1 Load Capacitance Selector
  4. 3Pullup Resistor Selector
    1. 3.1 Board Layout
  5. 4Schematic
    1. 4.1 Bill of Materials

EVM Setup

The following equipment is needed to evaluate the TCA9416:

  • Power supply capable of supplying the desired voltage to the TCA9416 and I2C bus
  • 4-channel oscilloscope to observe I2C transactions on both sides of the TCA9416
  • Microcontroller, processor, or digital analyzer which can send and receive I2C