SCEA119 September   2022 TMUX4051 , TMUX4052 , TMUX4053

 

  1.   Abstract
  2.   Trademarks
  3. 1Logic Compatibility
    1. 1.1 VIH Compatibility
    2. 1.2 VIL Compatibility
  4. 2Logic Outputs Levels vs. Input Control Logic Thresholds by Family

VIL Compatibility

Similarly, the low-level logic compatibility can be determined the same way through an understanding of the system and a side by side comparison of the VOL/VIL thresholds. To examine the VIL thresholds of the multiplexer, we will first need to discuss the VOL output voltage that comes from the driver. The VOL voltage is the voltage that is output by the driver when a low logic state is the desired outcome. Typically, there will be some maximum value provided in the driver’s data sheet and will be associated with certain conditions to achieve these output levels (for example, current). The voltage driven to produce a logic Low is ideally close to 0 V, but due to leakage currents, 0 V won’t necessarily be achieved. The leakage and actual voltage level on the node will be determined based on the architecture of the output driver. In a well-designed system, this VOL level will be close to 0 V varying only by mV’s. Because of this, often times system designers will overlook the VIL threshold and mainly focus on the VOH/VIH levels instead with the understanding that the VIL threshold compatibility will not play a significant role when it comes to the overall logic compatibility of the device in most scenarios.

To illustrate the VOL/VIL logic compatibility, use the TMUX405x with 1.8 V logic compatible feature with the minimum VIL equal to 0.8 V driven by a 5-V CMOS or 5 V TTL driver. Figure 1-2 shows that both the 5-V CMOS and 5-V TTL driver works because the maximum 0.5 V VOH is less than the maximum 0.8 V VIL. The TMUX405x read this as a low input, indicating that the old driver used with the existing CD405xB or CD74HCx405x are logic-low compatible with the new TMUX405x

Figure 1-2 TMUX405x Output Low Compatibility with 5-V CMOS and 5-V TTL Drivers