SCDU029 December   2021 TMUX4051 , TMUX4052 , TMUX4053

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Information About Cautions and Warnings
  5. 3Features
  6. 4 TMUXBQB-DYYEVM Header Connections and Test Points
  7. 5 TMUXBQB-DYYEVM Setup
  8. 6Layout
  9. 7Schematics
  10. 8Bill of Materials

TMUXBQB-DYYEVM Header Connections and Test Points

There are 16 headers located around the board with designators J1 through J16. These 3-by-2 headers serve as connections to power planes and to signals of the DUT (U1). Each pin of the DUT has similar header and test point configuration. At four different locations around the board, a legend shows the connections of the pins of the nearby five headers. Figure 4-1 shows a representation of the header associated with pin 3 of U1.

GUID-20211201-SS0I-K96Q-WWGN-5BGJ2RRN7WFP-low.jpgFigure 4-1 Header J3 for U1.3

The silkscreen legend represents the connections of the pins of J2. Figure 4-2 shows the pin numbers of this header from this same perspective.

GUID-C73B20E1-208C-4B6F-AC56-A6884A1EE0FF-low.pngGUID-CDEC3F74-3054-4286-BC27-3C6F96095F9B-low.pngFigure 4-2 Pinout of Headers

Table 4-1 also shows the connections.

Table 4-1 Connections by Header Pin Number
Header pin numberConnection
1No connection
2VDD
3GND
4U1
5GND
6VSS

For all headers J1 through J16, the connections are the same, but are rotated by a multiple of 90° according to their position on the board. A legend is included for each rotation.

In addition to headers, multiple test points are located around the board. Black test points (TP18 and TP20-TP26) are connected to GND, the red test point (TP17) is connected to VDD, and the green test point (TP19) is connected to VSS. The remaining blue test points (TP1-TP16 and TP101-TP116) are connected along the signal paths of the pins of U1.

GUID-20211201-SS0I-QP81-J1CC-RSRZZTCNRMLD-low.jpgFigure 4-3 Test Point Colors

Table 4-2 shows the test point connections.

Table 4-2 Test Point Connections
DesignatorConnection
TP1

J1.4

TP2

J2.4

TP3

J3.4

TP4

J4.4

TP5

J5.4

TP6

J6.4

TP7

J7.4

TP8

J8.4

TP9

J9.4

TP10

J10.4

TP11

J11.4

TP12

J12.4

TP13

J13.4

TP14J14.4
TP15

J15.4

TP16J16.4
TP17

VDD

TP18

GND

TP19VSS
TP20GND
TP21GND
TP22GND
TP23GND
TP24GND
TP25GND
TP26GND
TP101U1.1
TP102U1.2
TP103U1.3
TP104U1.4
TP105U1.5
TP106U1.6
TP107U1.7
TP108U1.8
TP109U1.9
TP110U1.10
TP111U1.11
TP112U1.12
TP113U1.13
TP114U1.14
TP115U1.15
TP116U1.16

Terminal block J18 is the power input for the board. Three power rails (VSS, GND, and VDD) are labeled on the board’s silkscreen layer, indicating the identities of the input pins of the header. Connect the power supply rails at this terminal block to power the board.