SBOK100 February   2025 SN54SC8T240-SEP , SN54SC8T244-SEP , SN54SC8T541-SEP , SN54SC8T9541-SEP

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Overview
  5. 2Single-Event Effects (SEE)
  6. 3Test Device and Test Board Information
  7. 4Irradiation Facility and Setup
  8. 5Results
    1. 5.1 SEL Results
    2. 5.2 Single-Event Transients (SET)
    3. 5.3 Event Rate Calculations
  9. 6Summary
  10. 7References

SEL Results

During SEL characterization, the device was heated using forced hot air, maintaining device temperature at 125°C. A FLIR (FLIR ONE Pro LT) thermal camera was used to validate die temperature to make sure the device was accurately heated (see Figure 4-2.) The species used for SEL testing was a Xenon (129Xe) ion at 25MeV / µ with an angle-of-incidence of 0° for an LETEFF of 50MeV-cm2/ mg. A fluence of approximately 1 × 107 ions / cm2 was used for each run.

The three devices were powered up and exposed to the heavy-ions using the maximum recommended supply voltage of 5.5V using a National Instruments™ PXI Chassis PXIe-4139 and a 5V, 1MHz square wave input using a National Instruments™ PXI Chassis PXIe-5423 function generator. The run duration to achieve this fluence was approximately 100 seconds. As listed in Table 5-2, no SEL events were observed during the nine runs, indicating that the SN54SC8T541-SEP is SEL-free. Figure 5-1, Figure 5-2, and Figure 5-3 show the plots of current versus time for runs two, six, and eight, respectively.

Table 5-1 Summary of SN54SC8T541-SEP SEL Test Conditions and Results
Run NumberUnit NumberDistance (mm)Temperature
(°C)
IonAngleFlux
(ions × cm2 / mg)
Fluence
(Number of ions)
LETEFF
(MeV × cm2/mg)
Did an SEL Event Occur?
1B870125Xe0°1.00E+051.00E+0750No
2B870125Xe0°1.00E+051.00E+0750No
3B870125Xe0°1.00E+051.00E+0750No

4

B970125Xe0°1.00E+051.00E+0750No

5

B970125Xe0°1.00E+051.00E+0750No

6

B970125Xe0°1.00E+051.00E+0750No

7

B1070125Xe0°1.00E+051.00E+0750No

8

B1070125Xe0°1.00E+051.00E+0750No

9

B1070125Xe0°1.00E+051.00E+0750No
 Current versus Time for Run 2 of the SN54SC8T541-SEP at T = 125°CFigure 5-1 Current versus Time for Run 2 of the SN54SC8T541-SEP at T = 125°C
 Current versus Time for Run 6 of the SN54SC8T541-SEP at T = 125°CFigure 5-2 Current versus Time for Run 6 of the SN54SC8T541-SEP at T = 125°C
 Current versus Time for Run 8 of the SN54SC8T541-SEP at T = 125°CFigure 5-3 Current versus Time for Run 8 of the SN54SC8T541-SEP at T = 125°C

No SEL events were observed, indicating that the SN54SC8T541-SEP is SEL-immune at LETEFF = 50MeV-cm2 / mg and T = 125°C. Using the MFTF method shown in Single-Event Effects (SEE) Confidence Internal Calculations , the upper-bound cross-section (using a 95% confidence level) is calculated as:

Equation 1. σSEL≤4.10×10-8cm2/device for LETEFF=50 MeV∙cm2/mg and T=125℃