SBOA626 December   2025 OPA187 , OPA192 , OPA202 , OPA320

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
    1. 1.1 Simple Analogy Explaining Instability
    2. 1.2 Circuits With Possible Stability Issues
    3. 1.3 Simple Stability Correction Based on Datasheet Plots
    4. 1.4 Introducing Lab Tools and Measurements
  5. 2Stability Theory for Operational Amplifiers
    1. 2.1 Poles and Zeros
    2. 2.2 Operational Amplifier Model Requirements for Stability Verification
    3. 2.3 Stability Definitions Based on Control Loop Model
    4. 2.4 Graphing Loop-Gain Based on AOL and 1/β
    5. 2.5 Rate of Closure Stability Test
    6. 2.6 Indirect (Non-Invasive) Stability Tests
  6. 3Simulating Open-Loop Stability Tests
    1. 3.1 Breaking the Loop the Wrong Way
    2. 3.2 Breaking the Loop With LC Test Circuit
    3. 3.3 Differential Loop Break Test
  7. 4Stability Correction for Capacitive Load
    1. 4.1 Isolation Resistor (RISO) Method
    2. 4.2 Dual Feedback Method
      1. 4.2.1 RISO-Dual-Feedback With RL
      2. 4.2.2 Dual Feedback With RFX Method
    3. 4.3 Snubber Circuit for Compensating Power Amplifiers and Reference Drive
    4. 4.4 Noise Gain for Stability Compensation
    5. 4.5 Feedback Capacitor (CF) Compensation for Capacitive Load
  8. 5Stability Corrections for Capacitance on the Inverting Node
    1. 5.1 Input Capacitance Instability Due to Zero in 1/β
    2. 5.2 Feedback Capacitor Solves Stability Issue for Capacitance on the Inverting Node
    3. 5.3 Minimum, Balanced, and Maximum Feedback Capacitance
    4. 5.4 Transimpedance Case
  9. 6Complex Open-Loop and Closed-Loop Output Impedance
    1. 6.1 Converting Open-Loop Output Impedance to Closed-Loop Output Impedance
    2. 6.2 Open-Loop and Closed-Loop Model Test
    3. 6.3 Instability Due to Resonance From Complex Output Impedance
    4. 6.4 Impact of Internal Op Amp Topology on Output Impedance Versus Frequency
    5. 6.5 Other Factors Effecting Output Impedance
  10. 7AOL Impact on Stability
    1. 7.1 AOL Secondary Poles and Zeros
    2. 7.2 Modeling the AOL Secondary Poles and Zeros and Input Capacitance
    3. 7.3 Decompensated Op Amps and Stability
    4. 7.4 The Impact of Closed-Loop Gain on Stability
  11. 8Common Problems in Stability Analysis
  12. 9References

Other Factors Effecting Output Impedance

The open-loop output impedance curve given in most op amp datasheets is a typical value. The datasheet typical value is also used in the op amp model. The ZO typical measurement was made at room temperature, with typical power supplies and load conditions. Factors such as output current, temperature, supply voltage, and process variations can cause ZO to change. Most datasheets do not provide estimates for worst case ZO, so targeting a conservative phase margin that remains stable even with some variation in ZO is advisable. This is why TI generally recommends a minimum phase margin of 45° even though 35° can potentially provide an acceptable transient response. Thus, if you design the circuit to a phase margin of 45°, across process and temperature the phase margin can potentially vary from 40° to 50°, which is generally acceptable.

Figure 6-22 illustrates how load current (amplifier output current) shifts ZO for OPA376. In general, ZO decreases for higher load current. Generally, the ZO curve in the datasheet is measured with minimal load current (large RL). For heavy loads (small RL), ZO decreases, which generally improves stability. Some amplifier datasheets, such as OPA376, show ZO for multiple different loads to show how ZO changes with load current.

OPA187 OPA202 OPA320 OPA192 Open-Loop Output Impedance Versus Load
          Current for
          OPA376 Figure 6-22 Open-Loop Output Impedance Versus Load Current for OPA376

Figure 6-23 illustrates an example of how ZO changes across temperature for PGA900. The PGA900 is used in the next few examples because the open-loop output impedance of PGA900 is characterized over a wide range of conditions that most devices are not tested under. While each amplifier has different characteristics and sensitivities, the PGA900 data provides a rough idea of what to expect. Figure 6-23 shows that temperature has a more significant effect at lower frequencies. In most circuits with stability concerns, the high frequency ZO determines the amplifier stability and low frequency ZO is not important. In this example, the curves are relatively tightly grouped past 10kHz (ΔZO(1MHz) ≅ ±20%).

OPA187 OPA202 OPA320 OPA192 Open-Loop Output Impedance Versus
          Temperature for
          PGA900 Figure 6-23 Open-Loop Output Impedance Versus Temperature for PGA900

The variation in ZO versus power supply voltage for PGA900 is really negligible (see Figure 6-24). This makes sense as op amps use internal biasing schemes that keep the bias current for the different internal blocks constant versus power supply voltage.

OPA187 OPA202 OPA320 OPA192 Open-Loop Output Impedance Versus
          Supply Voltage for
          PGA900 Figure 6-24 Open-Loop Output Impedance Versus Supply Voltage for PGA900

Figure 6-25 shows the process variation of ZO for PGA900. The data was collected for multiple different devices across multiple lots and the curves represent the worst-case deviations. As with other curves in this section, the variations at high frequency are not that significant, so the overall impact on stability is not that significant.

OPA187 OPA202 OPA320 OPA192 Open-Loop Output Impedance Versus
          Process for
          PGA900 Figure 6-25 Open-Loop Output Impedance Versus Process for PGA900

Figure 6-26 and Figure 6-27 illustrate the importance of decoupling for stability of op amps. Figure 6-26 shows the test circuit for measuring ZO. The circuit has a source impedance in the amplifier power supplies labeled RPS. This can be an inductive reactance, but for simplicity a resistance was used. With decoupling capacitors C2 and C3 installed, the power supply resistance is effectively shorted out from an AC perspective. If the decoupling is omitted, the resistance RPS effectively adds to the open-loop output impedance ZO. This is why improper decoupling or lack of decoupling often leads to op amp instability. Figure 6-27 illustrates measured ZO for OPA827 with the decoupling removed and resistor RPS added to the supply. Inspecting the graph shows that the source resistance increases the open-loop output impedance. The key point here is that this measurement was made without decoupling capacitors. Adding the decoupling effectively shorts out RPS so that all the ZO values match the original ZO regardless of RPS. Thus, decoupling capacitors are very important from a stability perspective. Use a minimum of 0.1µF decoupling with short connections between the amplifier supply pins and ground for good stability.

OPA187 OPA202 OPA320 OPA192 Open-Loop Output Impedance Test Versus
          Source Impedance and Decoupling Figure 6-26 Open-Loop Output Impedance Test Versus Source Impedance and Decoupling
OPA187 OPA202 OPA320 OPA192 Open-Loop Output Impedance Versus
          Supply Impedance for
          OPA827 Figure 6-27 Open-Loop Output Impedance Versus Supply Impedance for OPA827

The intention of this section is to emphasize that process, load, temperature, and decoupling all impact ZO and stability. Since most amplifier data sheets and associated SPICE models use the typical value for ZO, having a design target for phase margin that is conservative is important so that the circuit remains stable across process and temperature. This is really the motivation behind the 45° general guidance.