SBOA558 November   2022 LMH6642 , LMH6643 , LMH6643Q-Q1 , LMH6644 , OPA2328 , OPA328

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2ADCs Voltage Reference Buffering Using OPAx328
  5. 3ADC Driver Using OPAx328 High-Speed Op Amp
  6. 41-GΩ Transimpedance Amplifier(TIA) Using OPAx328
  7. 5Summary

1-GΩ Transimpedance Amplifier(TIA) Using OPAx328

The wide gain-bandwidth, low input bias current and low input voltage/current noise make the OPAx328 an excellent choice for implementation of the high gain transimpedance amplifier. However, photodiode junction capacitance, Cj, together with the desired trans-impedance gain, total output noise and bandwidth are important factors to be considered before deciding what circuit topology to use, see Figure 4-1.

GUID-20220825-SS0I-5KCZ-JJ6J-W22RGZRT5V8G-low.jpgFigure 4-1 1-GΩ TIA Options Using OPAx328

The simplest implementation of the transimpedance amplifier may be accomplished by use of a single feedback resistor (RG) to set its gain. However, 1-GΩ gain requires RG of 1 GΩ, which may not be practical because it could be higher than the parallel impedance of photodiode itself resulting in high gain error. Assuming photodiode impedance is much higher than 1-GΩ, you still need to make sure that the application circuit is stable. Since (Cj+Cin)||RG form a zero in 1/beta at fz=12π×RG×(Cin+Cj)=~12π×109×10-9=159mHz, it must be flatten with a pole before intersecting AOL, see Figure 4-2. Selecting CF of 1 pF forms a pole in transimpedance gain limiting the bandwidth to 159 Hz, fP=12π×109×10-12. This results in the phase margin of 89 degrees whereas the minimum 45 degrees is needed to assure stable operation of the circuit over process variation.

GUID-20220825-SS0I-THVL-H0GM-S45XSPR67NTG-low.jpgFigure 4-2 1-GΩ TIA AC Stability Using OPAx328

Performing a small-signal transient simulation shows overshoot of just few percent, see Figure 4-3. This confirms a very stable operation of the 1-GΩ TIA.

GUID-20220929-SS0I-50VG-R5KV-CGX1GJQZNSB8-low.pngFigure 4-3 1-GΩ TIA Transient Stability Using OPAx328

If the photodiode impedance is lower than 1-GΩ but much higher than 1-MΩ, one may implement the 1-GΩ transimpedance gain as a composite of 1-MΩ RG and an additional inner-loop gain of 1,000-V/V (R2/R1), as Figure 4-4 shows. However, using RG of 1-MΩ together with Cj of 1 nF forms a zero,fz=12π×RG×(Cin+Cj)=~12π×106×10-9=159Hz Thus, as was the case in Figure 4-2, in order to assure stability one must add CF to flatten the 1/beta before intersecting AOL. Adding CF of 100 pF creates a pole at 1,592 Hz, fP=12π×106×100×10-12, resulting in 70 degrees phase margin, Figure 4-4. This also leads to the increase of the TIA effective bandwidth by one-order of magnitude.

GUID-20220825-SS0I-NP1R-9QDH-VTG3FK1M9M0L-low.jpgFigure 4-4 1-GΩ TIA in Noise Gain of 1000 AC Stability Using OPAx328

Conducting a small-signal transient analysis shows overshoot of just 10 percent, which confirms stable operation of the composite 1-GΩ transimpedance amplifier, see Figure 4-5.

GUID-20220825-SS0I-6HXF-RTRG-K9X2QJRLVJVR-low.jpgFigure 4-5 1-GΩ TIA (in Noise Gain of 1000) Transient Stability Using OPAx328

Since the implementations of the previously-documented composite 1-GΩ TIA results in vastly higher voltage noise gain and bandwidth than the approach taken in Figure 4-3, this significantly increases the total output noise, which must be taken into consideration to arrive at the most optimal solution - see Figure 4-6.

GUID-20220825-SS0I-CZ46-2MBQ-HGGWSCZRPLTN-low.jpgFigure 4-6 Effect of 1-GΩ TIA Implementation on the Total Output Noise