SBAU260 April   2016

 

  1.   Delta-Sigma ADC EvaluaTIon Software User Manual
    1.     Trademarks
    2. 1  Glossary and Abbreviations
      1. 1.1 Abbreviations
      2. 1.2 Glossary
    3. 2  Installation
      1. 2.1 Core Application Installation
      2. 2.2 Device Package
      3. 2.3 Driver Installation
        1. 2.3.1 Automatic Installation
        2. 2.3.2 Manual Driver Installation
          1. 2.3.2.1 Automated Manual Driver Installation
          2. 2.3.2.2 Manual Driver Installation
    4. 3  Software Startup
      1. 3.1 Startup Screen (No Hardware Connected)
      2. 3.2 Startup Screen (Hardware Connected)
    5. 4  Application Window
      1. 4.1 Application Menu
      2. 4.2 Main Display Area
      3. 4.3 Status Bar
    6. 5  File Menu
      1. 5.1 Master Log Browser
      2. 5.2 About
        1. 5.2.1 Software User Guide
        2. 5.2.2 Application Support
          1. 5.2.2.1 Email Address
          2. 5.2.2.2 Attachments
          3. 5.2.2.3 Subject
          4. 5.2.2.4 Message
            1. 5.2.2.4.1 Sending the Email
      3. 5.3 Options
        1. 5.3.1 General Options
          1. 5.3.1.1 User Directory Controls
          2. 5.3.1.2 Register Update Operation
          3. 5.3.1.3 Console Tab Enable
        2. 5.3.2 Log Settings Options
          1. 5.3.2.1 Log Newline Inclusion
          2. 5.3.2.2 Log Settings
        3. 5.3.3 Command Delay Timing Options
        4. 5.3.4 Default Delay for Commands
        5. 5.3.5 COMMANDLIST Command Delay
        6. 5.3.6 REGMAP Command Delay
    7. 6  Device Tab
      1. 6.1 Device Tab Menu
        1. 6.1.1 Register Map Menu Group
          1. 6.1.1.1 Save
          2. 6.1.1.2 Load
          3. 6.1.1.3 Save Header
        2. 6.1.2 Application Clients Menu Group
          1. 6.1.2.1 Tools Menu
          2. 6.1.2.2 Additional Interfaces
          3. 6.1.2.3 Data Analysis
        3. 6.1.3 Documentation Menu Group
      2. 6.2 Operation
        1. 6.2.1 Register Map Table
        2. 6.2.2 Register Controls
        3. 6.2.3 Hardware Controls
        4. 6.2.4 Refresh/Sync and Write Defaults Controls
        5. 6.2.5 Register Decode and Information
        6. 6.2.6 Synchronous Manual Write
    8. 7  Script Tab
      1. 7.1 Script Tab Menu
        1. 7.1.1 Script File IO Menu Group
          1. 7.1.1.1 Save
          2. 7.1.1.2 Import
          3. 7.1.1.3 New
          4. 7.1.1.4 Rescan
        2. 7.1.2 Available Scripts Menu Group
          1. 7.1.2.1 Pre-Defined
          2. 7.1.2.2 User
        3. 7.1.3 Available Clients Menu Group
        4. 7.1.4 Documentation Menu Group
      2. 7.2 Operation
        1. 7.2.1 Script Information
        2. 7.2.2 Script Controls
          1. 7.2.2.1 Run Operation
          2. 7.2.2.2 Step Operation
          3. 7.2.2.3 Reset Button
        3. 7.2.3 Script Editing
          1. 7.2.3.1  Enabling Script Editing
          2. 7.2.3.2  Arrow Buttons
          3. 7.2.3.3  Available Commands
          4. 7.2.3.4  Available Command Help
          5. 7.2.3.5  Command Message Field
          6. 7.2.3.6  Command Description Field
          7. 7.2.3.7  Clear Button
          8. 7.2.3.8  Add New Button
          9. 7.2.3.9  Update Button
          10. 7.2.3.10 Delete Button
        4. 7.2.4 Activity Log
    9. 8  Console Tab
      1. 8.1 Console Tab Menu
        1. 8.1.1 Available Clients Group
        2. 8.1.2 Devices
        3. 8.1.3 Documentation Group
      2. 8.2 Operation
        1. 8.2.1 Command Controls
          1. 8.2.1.1 Device Commands
          2. 8.2.1.2 Command to Send Field
          3. 8.2.1.3 Send Command
        2. 8.2.2 Activity Log
    10. 9  Data Analysis Tool and Data Acquisition
      1. 9.1 Data Acquisition Process
        1. 9.1.1 Begin the Collection Process
        2. 9.1.2 Viewing the Data
      2. 9.2 Data Analysis Tool
        1. 9.2.1 General Controls Region
          1. 9.2.1.1 Channel Selection
          2. 9.2.1.2 EVM Parameters
          3. 9.2.1.3 Collect Controls
        2. 9.2.2 File Menu
          1. 9.2.2.1 About
          2. 9.2.2.2 Options
        3. 9.2.3 Data Inspector Tab
          1. 9.2.3.1 Data Display
          2. 9.2.3.2 Menu
            1. 9.2.3.2.1 Save Data As... Menu Option
        4. 9.2.4 Data Analysis Tab
          1. 9.2.4.1 Available Analysis Tools
          2. 9.2.4.2 Time Domain Analysis
            1. 9.2.4.2.1 Time Domain Options
            2. 9.2.4.2.2 Time Domain Graph
        5. 9.2.5 Log
    11. 10 Master Log Browser
      1. 10.1 Filtering the Log
      2. 10.2 Saving the Log
      3. 10.3 Creating Scripts From the Master Log
  2. AFrequently Asked Questions (FAQs)
    1. A.1 What if the hardware is not recognized by the software?
    2. A.2 I don't see any way to collect data! How can I do this?
    3. A.3 Can I manually enter commands in the software?
    4. A.4 Are there any additional analysis available, such as FFT or histogram?
    5. A.5 I created a script but it does not appear in the menu item?
  3. BScripts
    1. B.1 Device Script Generic Rules
    2. B.2 Device Script Node Description
    3. B.3 Device Script Example
  4. CRegister Map Files
    1. C.1 Register Map Files
    2. C.2 Register Map Settings File
    3. C.3 Register Map Header File
  5. DData File – Standard File Format
    1. D.1 Standard File Example

Time Domain Options

The Time Domain analysis provides several options to manipulate and change the displayed data.

The Points to Display control allows the user to specify the number of points to display on the graph. This number can be less than the total points collected to allow the user to look at a smaller portion of the data. If the number is larger than the points specified to collect, all the points collected are displayed. The points are always displayed beginning from the first data point in the array.

The Display value as: control allows for the data to be displayed as:

  • Volts (Input Referred)
  • Volts
  • Codes

Note that the Volts (Input Referred) option is provided for data channels that may have gain or digital scaling active. If the gain or digital scaling equals 1, then the two Volt options will show the same graph.