SBAA551 June   2022 ADS8661 , ADS8665 , ADS8671 , ADS8675 , ADS8681 , ADS8685 , ADS8689 , ADS8691 , ADS8695 , ADS8699 , INA823 , INA826 , LM317L , LM337L , MUX509 , TPS2661 , TPS560430

 

  1.   Abstract
  2.   Trademarks
  3. 1Introduction
  4. 2Circuit Description
    1. 2.1 Input Stage
    2. 2.2 Multiplexer Stage
    3. 2.3 Instrumentation Amplifier
    4. 2.4 Analog-to-Digital Converter
    5. 2.5 Power Supply
  5. 3Results
    1. 3.1 Accuracy and Noise Performance
    2. 3.2 Common-Mode Rejection of Input Signal
    3. 3.3 Input Impedance
    4. 3.4 Settling Time
    5. 3.5 Input Protection
  6. 4Summary
  7. 5References

Settling Time

Settling time specifies the time it takes to switch from one input channel (here: ch1) to another input channel (here: ch2) and the newly selected channel has settled across the analog front-end. The settling time is dictated mainly by the 2nd-order LPF inside the ADC. The preceding front-end should be fast enough not to influence the LPF settling time. This is achieved when a settled signal for each channel is available at the MUX input and settling after the MUX is reduced to a minimum.

Worst case, the input signal of the last channel is the opposite of the new channel, here VIN_DIFF_CH1 = –10 V and VIN_DIFF_CH2 = 10 V. Both channels are continuously and alternating converted. Only if both channels reach their steady state values (compare table 3 for steady state values for –10-V and +10-V input signals) the settling is considered complete. Due to demonstration software limitations, a sampling frequency of 24 kSPS (instead of 8 kSPS) was selected. Consequently, the 3rd conversion after each new channel selection is valid. The following image shows the proper settling within 115 μs (125μs (equals 8 kSPS) -10 μs (conversion time)) as the steady-state code for each channel (table 3) matches the codes in the lower-right corner.

GUID-20220610-SS0I-J3SJ-TTBJ-LRLPWVBM00LB-low.pngFigure 3-2 Settling Time Verification