DLPU110B April   2021  â€“ August 2022 DLPC6540

 

  1.   Programmer's Guide
  2.   Trademarks
  3. 1 Scope
  4. 2 References
  5. 3 Acronyms
  6. 4 System Boot
    1. 4.1 Data In flash
    2. 4.2 Bootloader Application
    3. 4.3 Main Application
    4. 4.4 Commands supported by Bootloader and Main Applications
    5. 4.5 Debug Terminal
    6. 4.6 HOST_IRQ/SYSTEM_BUSY
    7. 4.7 Heartbeat
    8. 4.8 Low-level Fault
  7. 5 System Status
  8. 6 Version
  9. 7 Power Modes
  10. 8 Display Modes
  11. 9 Source Detection and Configuration
  12. 10Internal sources
    1. 10.1 Test Patterns (TPG)
    2. 10.2 Solid Field (SFG) Color
    3. 10.3 Curtain
  13. 11Display Formatting
  14. 12Image Processing
  15. 13Illumination Control
  16. 14Peripherals
    1. 14.1 GPIO
  17. 15Interface Protocol
    1. 15.1 Supported Interfaces
    2. 15.2 I2C Target
    3. 15.3 USB
  18. 16Command Protocol
    1. 16.1 Command Packet
    2. 16.2 Response Packet
    3. 16.3 Destination Details
    4. 16.4 Error Handling and Recovery
    5. 16.5 System Busy - I2C scenarios
      1. 16.5.1 GPIO implementation
      2. 16.5.2 Short Status response
    6. 16.6 Support for Variable Data Size
  19. 17Auto-Initilization Batch File
  20. 18Command Descriptions
  21. 19 System Commands
    1. 19.1  3D
    2. 19.2  Administrative
    3. 19.3  Autolock
    4. 19.4  Blending
    5. 19.5  Bootloader
    6. 19.6  Calibration
    7. 19.7  Debug Internal
    8. 19.8  Debug
    9. 19.9  General Operation
    10. 19.10 Illumination
    11. 19.11 Image Processing
    12. 19.12 Peripherals
    13. 19.13 Warping
    14. 19.14 Manual WPC
  22. 20Revision History

Blending

Blending

Table 19-21 Blend Map Gain Values [Opcode: 2Bh | Destination: 4]
Set Blend Map Gain Values
Write Parameter(s)
Byte Description
Byte 0

Compressed Values Passed

bit0: 1 = Compressed data is passed below for Gain values.

0 = Uncompressed data is passed below for Gain values.

Byte 1

Color Channel Select

0 = Broadcast

1 = Green

2 = Red

3 = Blue

Bytes 2-3

Here the total number of compressed values needs to be passed only when CompressionEnable is Enabled otherwise pass 0 here

Bytes 4-5

Starting Index for filling the Gain values in array of Gain

Bytes 6 - *

Gain of control points .The format of input should be such that required gain which is a value between 0 to 1.99 be multiplied by 4096 before passing it in command.

This command takes the user given gain values of control points as part of the Blend Map. Using this command user passes the Gain values for the 2016 (63x32) control points. The gain values needs to be specified for each of the color channel.

There are two features here for using the command. User can select the broadcast values option from the Color Channel Select. What broadcast does is that user needs to pass values only once and it will broadcasted to all the three color channels R,G,B. Otherwise user needs to pass value for R, G, B color channels separately. So the command will then be required to use 3 times one time for each color channel Another feature supported is passing compressed values. The compression used is RLE2 compression. For passing compressed values user needs to enable the Compression Enabled bit

Get Blend Map Gain Values
Read Parameter(s)
Byte Description
Byte 0

Color Channel Select

0 = Broadcast

1 = Green

2 = Red

3 = Blue

Bytes 1-2

Start index in the Blend map channel gain values from which the data is to be read

Bytes 3-4

Number of entries to be read

Return Parameter(s)
Byte Description
Byte 0

This tells whether the gain values obtained are compressed data or not.

Bytes 1 - *

Selected Color Channel gain values

This command reads from the blend map table already loaded using Set Blend Map Gain Values command. N Blend map gain values (that does not exceed the command packet size) can be read at a time from anywhere within the table.

Table 19-22 Apply Blend Map [Opcode: 2Ch | Destination: 4]
Set Apply Blend Map
Write Parameter(s)
Byte Description
Byte 0

Blend Map Upload

bit0: 1 = Blend Map values is enabled and applied.

0 = Blend Map values is disabled.

This command is used to apply the Blend map with the given configuration

Table 19-23 Blend Map Offset Values [Opcode: 2Dh | Destination: 4]
Set Blend Map Offset Values
Write Parameter(s)
Byte Description
Byte 0

Compressed Values Passed

bit0: 1 = Compressed data is passed below for Offset values.

0 = Uncompressed data is passed below for Offset values.

Byte 1

Color Channel Select

0 = Broadcast

1 = Green

2 = Red

3 = Blue

Bytes 2-3

Here the total number of compressed values needs to be passed only when the first parameter is 1 otherwise pass 0 here

Bytes 4-5

Starting Index for filling the Offset values in array

Bytes 6 - *

Offset of control points.The format of input should be such that the offset values are in the internal floating point format of s1m8e4 .

Using this command user passes the Offset values for the 2016 (63x32) control points. The Offset values needs to be specified for each of the color channel R,G,B. The range of offset values in the standard floating point format is -255 to +255.

There are two features here for using the command. User can select the broadcast values option from the Color Channel Select. What broadcast does is that user needs to pass values only once and it will broadcasted to all the three color channels R,G,B. Otherwise user needs to pass value for R, G, B color channels separately. So the command will then be required to use 3 times one time for each color channel.

Another feature supported is passing compressed values. The compression used is RLE2 compression. For passing compressed values user needs to enable the Compression Enabled bit

Get Blend Map Offset Values
Read Parameter(s)
Byte Description
Byte 0

Color Channel Select

0 = Broadcast

1 = Green

2 = Red

3 = Blue

Bytes 1-2

Start index in the Blend map channel Offset values from which the data is to be read

Bytes 3-4

Number of entries to be read

Return Parameter(s)
Byte Description
Byte 0

This tells whether the offset values obtained are compressed data or not.

Bytes 1 - *

Selected Color Channel Offset

This command reads from the blend map compressed offset values already loaded using Set Blend Map Offset Values command. N Blend map offset values (that does not exceed the command packet size) can be read at a time from anywhere within the table.

Table 19-24 Blend Map Control Points [Opcode: 2Eh | Destination: 4]
Set Blend Map Control Points
Write Parameter(s)
Byte Description
Bytes 0-1

Horizontal Display Resolution of Projector

Bytes 2-3

Vertical Display Resolution of Projector

Bytes 4 - *

Blend Map Horizontal control points position array

Number of points in this array equal to 63.These control points are 0 based.

Bytes 4 - *

Blend Map Vertical control points position array

Number of points in this array equal to 32.These control points are 0 based.

This command takes input of the user defined control points location in horizontal and vertical direction as part of the Blend Map

Get Blend Map Control Points
Return Parameter(s)
Byte Description
Bytes 0-125

Blend map Horizontal control points position array.

Number of points in this array equal to IMG_BLENDMAP_CTL_POINTS_X

Bytes 126-189

Blend map Vertical control points position array.

Number of points in this array equal to IMG_BLENDMAP_CTL_POINTS_Y

This command gets the user defined blend map control points location stored in EEPROM.

Table 19-25 Enable Edge Blending [Opcode: 2Fh | Destination: 4]
Set Enable Edge Blending
Write Parameter(s)
Byte Description
Byte 0

EBF State

bit0: 1 = Edge blending is enabled

0 = Edge blending is disabled

This command enables or disables the Edge blending function

Get Enable Edge Blending
Data returned is in the same format as the Write Parameter(s).

Returns whether the Edge blending function is enabled or not.

Table 19-26 Edge Blending System Params [Opcode: 3Dh | Destination: 4]
Set Edge Blending System Params
Write Parameter(s)
Byte Description
Bytes 0-1

Number of columns of projectors in blending system

Range = 1 to 32 with step size 1

Bytes 2-3

Number of rows of projectors in blending system

Range = 1 to 32 with step size 1

Bytes 4-5

Column index of self in blending system

Range = 0 to 31 with step size 1

Bytes 6-7

Row index of self in blending system

Range = 0 to 31 with step size 1

Bytes 8 - *

White and black luminance levels of projectors in blending system, raster scan order. Format is fixed point 16.16

(nits)

This command sets the blending system parameters for semi-manual edge blending. This command does not change the state of the warping map or the blending map

Get Edge Blending System Params
Data returned is in the same format as the Write Parameter(s).

This command gets the blending system parameters for semi-manual edge blending

Table 19-27 Edge Blending Configuration [Opcode: 3Eh | Destination: 4]
Set Edge Blending Configuration
Write Parameter(s)
Byte Description
Bytes 0-1

Horizontal Overlap with other projectors

(pixels)

Bytes 2-3

Vertical Overlap with other projectors

(pixels)

Byte 4

Geometric Adjustment Type

0 = No Geometric Correction

1 = Keystone Corners

Byte 5

Storage Options

0 = Dont Store

1 = Write To Storage

2 = Write To Storage Apply At Startup

Bytes 6 - *

Geometric adjustment parameters. Dependent on adjustment type used

This command sets overlap and geometry parameters for semi-manual edge blending, creates and applies blending and warping maps for given blending inputs. It is necessary to call commands to enable manual warping and enable edge blending separately, for the results to take effect.

Geometry parameters are dependent on geometric adjustment type. For no geometric correction, no parameters are used. For correction by keystone corners, the 8 parameters are the (x,y) coordinates (zero based) of the keystone corners in raster scan order : top-left, top-right, bottom-left, bottom-right.

Get Edge Blending Configuration
Data returned is in the same format as the Write Parameter(s).

This command gets geometry and overlap parameters for semi-manual edge blending. Geometry parameters are dependent on geometric adjustment type. For no geometric correction, no parameters are used. For correction by keystone corners, the 8 parameters are the (x,y) coordinates (zero based) of the keystone corners in raster scan order : top-left, top-right, bottom-left, bottom-right.