DLPU058A September 2017 – February 2019
The DLP LightCrafter Display 3010 EVM-G2 is composed of three parts:
The main board contains the connector for the power supply, a USB connector to communicate to the DLP LightCrafter Display software, HDMI and the connector for the DLP LightCrafter Display board. The main board also contains a switch to turn on the projector in case the DLP LightCrafter Display board and the engine are connected. Figure 5 shows the main connectors on the main board.
Figure 5. DLP LightCrafter Display Main Board The DLP LightCrafter Display board contains the RGB LED connectors, the Flex cable connector, and the main board connector. To connect the main board to the DLP LightCrafter Display board, refer to Figure 6. Note that the main board connector on the DLP LightCrafter Display board is on the bottom, while the LED and Flex cable connectors are on the top.
Figure 6. Connection Main Board and DLP LightCrafter Display Board Figure 7 shows the display board and how it connects to the main board. The different connectors for each LED are named on the board as well as on the light engine.
Figure 7. DLP LightCrafter Display EVM Ensure a good connection of the flex cable and LED cables to the DLP LightCrafter Display board before turning it on.