ZHCSNM7 March 2021 TPSM13604H
PRODUCTION DATA
The TPSM13604 module contains an internal 0.47-µF input ceramic capacitor. Additional input capacitance is required externally to the module to handle the input ripple current of the application. This input capacitance must be as close as possible to the module. Input capacitor selection is generally directed to satisfy the input ripple current requirements rather than by capacitance value.
Worst-case input ripple current rating is dictated by Equation 12.
where
As a point of reference, the worst-case ripple current occurs when the module is presented with full load current and when VIN = 2 × VO.
Recommended minimum input capacitance is 10-µF X7R ceramic with a voltage rating at least 25% higher than the maximum applied input voltage for the application. TI also recommends to pay attention to the voltage and temperature deratings of the capacitor selected. Note that ripple current rating of ceramic capacitors can be missing from the capacitor data sheet and you may have to contact the capacitor manufacturer for this rating.
If the system design requires a certain maximum value of input ripple voltage ΔVIN to be maintained, then Equation 13 can be used.
If ΔVIN is 2% of VIN for a 12-V input to a 9-V output application this equals 120 mV and fSW = 300 kHz.
Additional bulk capacitance with higher ESR can be required to damp any resonant effects of the input capacitance and parasitic inductance of the incoming supply lines.