ZHCSMV2A December 2020 – December 2021 TPS55288-Q1
PRODUCTION DATA
Figure 5-1 26-pin
VQFN-HR, RPM Package (Transparent Top
View)| PIN | I/O | DESCRIPTION | |
|---|---|---|---|
| NO. | NAME | ||
| 1 | DR1L | O | Gate driver output for low-side MOSFET in buck side |
| 2 | DR1H | O | Gate driver output for high-side MOSFET in buck side |
| 3 | VIN | PWR | Input power supply for the IC |
| 4 | EN/UVLO | I | Enable logic input and programmable input voltage undervoltage lockout (UVLO) input. Logic high level enables the device. Logic low level disables the device and turns it into shutdown mode. After the voltage at the EN/UVLO pin is above the logic high voltage of 1.15 V, this pin acts as programmable UVLO input with 1.23-V internal reference. |
| 5 | SCL | I | Clock of I2C interface |
| 6 | SDA | I/O | Data of I2C interface |
| 7 | DITH/SYNC | I | Dithering frequency setting and synchronous clock input. Use a capacitor between this pin and ground to set the dithering frequency. When this pin is short to ground or pulled above 1.2 V, there is no dithering function. An external clock can be applied at this pin to synchronize the switching frequency. |
| 8 | FSW | O | The switching frequency is programmed by a resistor between this pin and the AGND pin. |
| 9, 24 | PGND | PWR | Power ground of the IC. It is connected to the source of the low-side MOSFET. |
| 10 | AGND | PWR | Signal ground of the IC |
| 11, 26 | VOUT | PWR | Output of the buck-boost converter |
| 12 | ISP | I | Positive input of the current sense amplifier. An optional current sense resistor connected between the ISP pin and the ISN pin can limit the output current. If the sensed voltage reaches the current limit setting value in the register, a slow constant current control loop becomes active and starts to regulate the voltage between the ISP pin and the ISN pin. Connecting the ISP pin and the ISN pin together with the VOUT pin can disable the output current limit function. |
| 13 | ISN | I | Negative input of the current sense amplifier. An optional current sense resistor connected between the ISP pin and the ISN pin can limit the output current. If the sensed voltage reaches the current limit setting value in the register, a slow constant current control loop becomes active and starts to regulate the voltage between the ISP pin and the ISN pin. Connecting the ISP pin and the ISN pin together with the VOUT pin can disable the output current limit function. |
| 14 | FB/INT | I/O | When the device is set to use external output voltage feedback, connect to the center tap of a resistor divider to program the output voltage. When the device is set to use internal feedback, this pin is a fault indicator output. When there is an internal fault happening, this pin outputs logic low level. |
| 15 | MODE | I | Set the operation modes of the TPS55288-Q1 by a resistor between this pin and AGND to select PFM mode, forced PWM mode in light load condition to select the internal LDO, or external 5 V for VCC, and to select different I2C address. |
| 16 | CDC | O | Voltage output proportional to the sensed voltage between the ISP pin and the ISN pin. Use a resistor between this pin and AGND to increase the output voltage to compensate voltage droop across the cable caused by the cable resistance. |
| 17 | ILIM | O | Average inductor current limit setting pin. Connect an external resistor between this pin and the AGND pin. |
| 18 | COMP | I | Output of the internal error amplifier. Connect the loop compensation network between this pin and the AGND pin. |
| 19 | VCC | O | Output of the internal regulator. A ceramic capacitor of more than 4.7 μF is required between this pin and the AGND pin. |
| 20 | BOOT2 | O | Power supply for high-side MOSFET gate driver in boost side. A ceramic capacitor of 0.1 µF must be connected between this pin and the SW2 pin. |
| 21, 25 | SW2 | I | The switching node pin of the boost side. It is connected to the drain of the internal low-side power MOSFET and the source of internal high-side power MOSFET. |
| 22 | BOOT1 | I | Power supply for high-side MOSFET gate driver in buck side. A ceramic capacitor of 0.1 µF must be connected between this pin and the SW1 pin. |
| 23 | SW1 | I | The switching node pin of the buck side. It is connected to the drain of the external low-side power MOSFET and the source of external high-side power MOSFET. |