ZHCSCR7A June 2014 – November 2020 TPS2559
PRODUCTION DATA
Some applications require that current limiting cannot occur below a certain threshold. For this example, assume that 3 A must be delivered to the load so that the minimum desired current-limit threshold is 3000 mA. Use the IOS equations and Figure 9-2 to select R(ILIM).

Select the closest 1% resistor less than the calculated value: R(ILIM) = 36.5 kΩ. This sets the minimum current-limit threshold at 3016 A.

Use the IOS equations, Figure 9-2, and the previously calculated value for R(ILIM) to calculate the maximum resulting current-limit threshold.

The resulting maximum current-limit threshold minimum is 3016 mA and maximum is 3387 mA with a 36.5 kΩ ± 1%.