ZHCSEK5A JANUARY 2015 – September 2018 TPL5110
PRODUCTION DATA.
The manual Power ON may be implemented using a switch (momentary mechanical action). The TPL5110 offers two possible approaches according to the power consumption constraints of the application.
Figure 13. Manual MOSFET Power ON With SPST Switch For use cases that do not require the lowest power consumption, using a single-pole single-throw switch may offer a lower-cost solution. The DELAY/M_DRV pin may be directly connected to VDD with REXT in the circuit. The current drawn from the supply voltage during the manual power ON is given by VDD/REXT.
Figure 14. Manual MOSFET Power ON With SPDT Switch The manual MOSFET Power ON function may also be asserted by switching DELAY/M_DRV from REXT to VDD using a single-pole double-throw switch, which will provide a lower power solution for the manual power ON, because no current flows.