SLVSK31 June 2026 TLV9023L
PRODUCTION DATA
There is a delay between when the input crosses the reference voltage and the output responds. This is called the Propagation Delay. This is shown as tpHL in Figure 7-1 and is measured from the mid-point of the input to the midpoint of the output. Because of the latch, the TLV9023L does not have a "Low-to high" (tpLH) specification. tpLH is replaced by the "Clear Fall to Latch Reset propagation delay time" (TPD-CLR-F) specification, which is the time between the falling edge of the CLR input and the rising edge of the output.