ZHCSDM7B February   2012  – December 2014 LMP8646
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
    5. 6.5 Electrical Characteristics: 2.7 V
    6. 6.6 Electrical Characteristics: 5 V
    7. 6.7 Electrical Characteristics: 12 V
    8. 6.8 Typical Characteristics
  7. Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
      1. 7.3.1 Theory of Operation
        1. 7.3.1.1 Maximum Output Voltage, VOUT_MAX
          1. 7.3.1.1.1 Case 1: −2 V < VCM < 1.8 V, and VS > 2.7 V
          2. 7.3.1.1.2 Case 2: 1.8 V < VCM < VS, and VS > 3.3 V
          3. 7.3.1.1.3 Case 3: VCM > VS, and VS > 2.7 V
    4. 7.4 Device Functional Modes
      1. 7.4.1 Output Accuracy
      2. 7.4.2 Selection of the Sense Resistor, RSENSE
        1. 7.4.2.1 RSENSE Consideration for System Error
  8. Application and Implementation
    1. 8.1 Application Information
    2. 8.2 Typical Applications
      1. 8.2.1 Application #1: Current Limiter With a Capacitive Load
        1. 8.2.1.1 Design Requirements
        2. 8.2.1.2 Detailed Design Procedure
        3. 8.2.1.3 Application Curve
      2. 8.2.2 Application #2: Current Limiter With a Resistive Load
        1. 8.2.2.1 Design Requirements
        2. 8.2.2.2 Detailed Design Procedure
        3. 8.2.2.3 Application Curve
      3. 8.2.3 Application #3: Current Limiter With a Low-Dropout Regulator and Resistive Load
        1. 8.2.3.1 Design Requirements
        2. 8.2.3.2 Detailed Design Procedure
        3. 8.2.3.3 Application Curve
  9. Power Supply Recommendations
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
  11. 11器件和文档支持
    1. 11.1 商标
    2. 11.2 静电放电警告
    3. 11.3 Glossary
  12. 12机械、封装和可订购信息

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

7 Detailed Description

7.1 Overview

The LMP8646 is a single-supply precision current limiter with variable gain selected through an external resistor (RG) and a variable bandwidth selected through an external capacitor (CG) in parallel with RG. Its common-mode of operation is –2 V to 76 V, and the LMP8646 has an buffered output to provide a low-output impedance. More details of the LMP8646's functional description can be seen in the following subsections.

7.2 Functional Block Diagram

LMP8646 30123530.gif

7.3 Feature Description

7.3.1 Theory of Operation

As seen from Figure 26, the sense current flowing through RSENSE develops a voltage drop equal to VSENSE. The high impedance inputs of the amplifier does not conduct this current and the high open-loop gain of the sense amplifier forces its noninverting input to the same voltage as the inverting input. In this way the voltage drop across RIN matches VSENSE. The current IIN flowing through RIN has the following equation:

Equation 1. IIN = VSENSE/ RIN = RSENSE*ISENSE/RIN

where

  • RIN = 1/Gm = 1/(200 µA/V) = 5 kOhm

IIN flows entirely across the external gain resistor RG to develop a voltage drop equal to:

Equation 2. VRG = IIN*RG = (VSENSE/RIN) *RG = [(RSENSE*ISENSE) / RIN]*RG


This voltage is buffered and showed at the output with a very low impedance allowing a very easy interface of the LMP8646 with the feedback of many voltage regulators. This output voltage has the following equation:

Equation 3. VOUT = VRG = [(RSENSE*ISENSE) / RIN]*RG
Equation 4. VOUT = VSENSE* RG/RIN
Equation 5. VOUT = VSENSE* RG/(5 kOhm)
Equation 6. VOUT = VSENSE* Gain

where

  • Gain = RG/RIN
LMP8646 30123503.gifFigure 26. Current Monitor

7.3.1.1 Maximum Output Voltage, VOUT_MAX

The maximum output voltage, VOUT_MAX, depends on the supply voltage, VS = V+ - V-, and on the common-mode voltage, VCM = (+IN + -IN) / 2.

The following subsections show three cases to calculate for VOUT_MAX.

7.3.1.1.1 Case 1: −2 V < VCM < 1.8 V, and VS > 2.7 V

  If VS ≥ 5 V,

  then VOUT_MAX = 1.3 V.

 Else if Vs = 2.7 V,

  then VOUT_MAX = 1.1 V.

7.3.1.1.2 Case 2: 1.8 V < VCM < VS, and VS > 3.3 V

In this case, VX is a fixed value that depends on the supply voltage. VX has the following values:

  If VS = 12 V, then VX = 10 V.

  Else if VS = 5 V, then VX = 3.3 V .

  Else if VS = 2.7 V, then VX = 1.1 V.

  If VX ≤ (VCM - VSENSE - 0.25) ,

  then VOUT_MAX = VX.

 Else,

  VOUT_MAX = (VCM - VSENSE - 0.25).

For example, if VCM = 4 V, VS = 5 V (and thus VX = 3.3 V), VSENSE = 0.1 V, then VOUT_MAX = 3.3 V because 3.3 V ≤ (4 - 0.1 - 0.25).

7.3.1.1.3 Case 3: VCM > VS, and VS > 2.7 V

 If VS = 12 V, then VOUT_MAX = 10 V.

 Else if VS = 5 V, then VOUT_MAX = 3.3 V .

 Else if VS = 2.7 V, then VOUT_MAX = 1.1 V.

7.4 Device Functional Modes

7.4.1 Output Accuracy

The output accuracy is the device error contributed by the LMP8646 based on its offset and gain errors. The LMP8646 output accuracy has the following equations:

Equation 7. LMP8646 30123538.gif
Output Accuracy Equations

For example, assume VSENSE = 100 mV, RG = 10 kOhm, and it is known that VOFFSET = 1 mV and Gm_Accuracy = 2% (Electrical Characteristics Table), then the output accuracy can be calculated as:

Equation 8. LMP8646 30123539.gif
Output Accuracy Example

In fact, as VSENSE decreases, the output accuracy worsens as seen in Figure 27. These equations provide a valuable tool to estimate how the LMP8646 affects the overall system performance. Knowing this information allows the system designer to pick the appropriate external resistances (RSENSE and RG) to adjust for the tolerable system error. Examples of this tolerable system error can be seen in the next sections.

LMP8646 30123570.gifFigure 27. Output Accuracy vs. VSENSE

7.4.2 Selection of the Sense Resistor, RSENSE

The accuracy of the current measurement also depends on the value of the shunt resistor RSENSE. Its value depends on the application and is a compromise between small-signal accuracy and maximum permissible voltage loss in the load line.

RSENSE is directly proportional to VSENSE through the equation RSENSE = (VSENSE) / (ISENSE). If VSENSE is small, then there is a smaller voltage loss in the load line, but the output accuracy is worse because the LMP8646 offset error will contribute more. Therefore, high values of RSENSE provide better output accuracy by minimizing the effects of offset, while low values of RSENSE minimize the voltage loss in the load line. For most applications, best performance is obtained with an RSENSE value that provides a VSENSE of 100 mV to 200 mV.

7.4.2.1 RSENSE Consideration for System Error

The output accuracy described in the previous section talks about the error contributed just by the LMP8646. The system error, however, consists of the errors contributed by the LMP8646 as well as other external resistors such as RSENSE and RG. Let's rewrite the output accuracy equation for the system error assuming that RSENSE is non-ideal and RG is ideal. This equation can be seen as:

Equation 9. LMP8646 30123554.gif
System Error Example Assuming RSENSE is Non-ideal and RG is Ideal

Continuing from the previous output accuracy example, we can calculate for the system error assuming that RSENSE = 100 mOhm (with 1% tolerance), ISENSE = 1A, and RG = 10 kOhm. From the Electrical Characteristics Table, it is also known that VOFFSET = 1 mV and Gm_Accuracy = 2%.

Equation 10. LMP8646 30123555.gif
System Error Example Assuming RSENSE is Non-ideal and RG is Ideal

Because an RSENSE tolerance will increase the system error, we recommend selecting an RSENSE resistor with low tolerance.