ZHCSGU1C September 2017 – October 2021 LM5150-Q1
PRODUCTION DATA
The input capacitors reduce the input voltage ripple. Assuming high-quality ceramic capacitors are used for the input capacitors, the maximum input voltage ripple can be calculated by using Equation 39.

The required input capacitor value is a function of the impedance of the source power supply. More input capacitors are required if the impedance of the source power supply is not low enough. In the example, three 10-µF ceramic capacitors are used.