ZHCSEU0A November   2015  – December 2015 LM5109B-Q1
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
    6. 6.6 Switching Characteristics
    7. 6.7 Typical Characteristics
  7. 7 Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
      1. 7.3.1 Start-up and UVLO
      2. 7.3.2 Level Shift
      3. 7.3.3 Output Stages
    4. 7.4 HS Transient Voltages Below Ground
    5. 7.5 Device Functional Modes
  8. 8 Application and Implementation
    1. 8.1 Application Information
    2. 8.2 Typical Application
      1. 8.2.1 Design Requirements
      2. 8.2.2 Detailed Design Procedure
        1. 8.2.2.1 Select Bootstrap and VDD Capacitor
        2. 8.2.2.2 Select External Bootstrap Diode and Its Series Resistor
        3. 8.2.2.3 Selecting External Gate Driver Resistor
        4. 8.2.2.4 Estimate the Driver Power Loss
      3. 8.2.3 Application Curves
  9. 9 Power Supply Recommendations
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
  11. 11器件和文档支持
    1. 11.1 社区资源
    2. 11.2 商标
    3. 11.3 静电放电警告
    4. 11.4 Glossary
  12. 12机械、封装和可订购信息

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

8 Application and Implementation

NOTE

Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.

8.1 Application Information

To operate fast switching of power MOSFETs at high switching frequencies and to reduce associated switching losses, a powerful gate driver is employed between the PWM output of controller and the gates of the power semiconductor devices. Also, gate drivers are indispensable when it is impossible for the PWM controller to directly drive the gates of the switching devices. With the advent of digital power, this situation is often encountered because the PWM signal from the digital controller is often a 3.3 V logic signal which cannot effectively turn on a power switch. Level shift circuit is needed to boost the 3.3 V signal to the gate-drive voltage (such as 12 V) in order to fully turn-on the power device and minimize conduction losses. Traditional buffer drive circuits based on NPN/PNP bipolar transistors in totem-pole arrangement prove inadequate with digital power because they lack level-shifting capability. Gate drivers effectively combine both the level-shifting and buffer-drive functions. Gate drivers also find other needs such as minimizing the effect of high-frequency switching noise (by placing the high-current driver IC physically close to the power switch), driving gate-drive transformers and controlling floating power-device gates, reducing power dissipation and thermal stress in controllers by moving gate charge power losses from the controller into the driver.

The LM5109B-Q1 is the high voltage gate drivers designed to drive both the high-side and low-side N-Channel MOSFETs in a half-bridge/full bridge configuration or in a synchronous buck circuit. The floating high side driver is capable of operating with supply voltages up to 90V. This allows for N-Channel MOSFETs control in half-bridge, full-bridge, push-pull, two switch forward and active clamp topologies. The outputs are independently controlled. Each channel is controlled by its respective input pins (HI and LI), allowing full and independent flexibility to control ON and OFF state of the output.

8.2 Typical Application

LM5109B-Q1 typical_application_snvsag6.gif Figure 14. LM5109B-Q1 Driving MOSFETs in a Half Bridge Converter

8.2.1 Design Requirements

Table 4. Design Example

PARAMETER VALUE
Gate Driver LM5109B-Q1
MOSFET CSD19534KCS
VDD 10 V
QG 17 nC
fSW 500 kHz

8.2.2 Detailed Design Procedure

8.2.2.1 Select Bootstrap and VDD Capacitor

The bootstrap capacitor must maintain the VHB-HS voltage above the UVLO threshold for normal operation. Calculate the maximum allowable drop across the bootstrap capacitor with Equation 1.

Equation 1. LM5109B-Q1 eq01_snvsag6.gif

where

  • VDD = Supply voltage of the gate drive IC;
  • VDH = Bootstrap diode forward voltage drop;
  • VHBL = VHBRmax – VHBH, HB falling threshold;

Then, the total charge needed per switching cycle could be estimated by Equation 2.

Equation 2. LM5109B-Q1 eq02_snvsag6.gif

where

  • QG: Total MOSFET gate charge
  • IHBS: HB to VSS Leakage current
  • DMax: Converter maximum duty cycle
  • IHB: HB Quiescent current

Therefore, the minimum CBoot should be:

Equation 3. LM5109B-Q1 eq03_snvsag6.gif

In practice, the value of the CBoot capacitor should be greater than calculated to allow for situations where the power stage may skip pulse due to load transients. It is recommended to have enough margins and place the bootstrap capacitor as close to the HB and HS pins as possible.

Equation 4. CBoot = 100 nF

As a general rule the local VDD bypass capacitor should be 10 times greater than the value of CBoot, as shown in Equation 5.

Equation 5. CVDD = 1 µF

The bootstrap and bias capacitors should be ceramic types with X7R dielectric. The voltage rating should be twice that of the maximum VDD considering capacitance tolerances once the devices have a DC bias voltage across them and to ensure long-term reliability.

8.2.2.2 Select External Bootstrap Diode and Its Series Resistor

The bootstrap capacitor is charged by the VDD through the external bootstrap diode every cycle when low side MOSFET turns on. The charging of the capacitor involves high peak currents, and therefore transient power dissipation in the bootstrap diode may be significant and the conduction loss also depends on its forward voltage drop. Both the diode conduction losses and reverse recovery losses contribute to the total losses in the gate driver circuit.

For the selection of external bootstrap diodes, please refer to the application note SNVA083A. Bootstrap resistor RBOOT is selected to reduce the inrush current in DBOOT and limit the ramp up slew rate of voltage of VHB-HS during each switching cycle, especially when HS pin have excessive negative transient voltage. RBOOT recommended value is between 2 Ω and 10 Ω depending on diode selection. A current limiting resistor of 2.2 Ω is selected to limit inrush current of bootstrap diode, and the estimated peak current on the DBoot is shown in Equation 6.

Equation 6. LM5109B-Q1 eq04_snvsag6.gif

where

  • VDH is the Bootstrap diode forward voltage drop

8.2.2.3 Selecting External Gate Driver Resistor

External Gate Driver Resistor, RGATE, is sized to reduce ringing caused by parasitic inductances and capacitances and also to limit the current coming out of the gate driver.

Peak HO pull-up current are calculated by the following equations.

Equation 7. LM5109B-Q1 eq05_snvsag6.gif

where

  • IOHH – Peak pull-up current;
  • VDH – Bootstrap diode forward voltage drop;
  • RHOH – Gate driver internal HO pull-up resistance, provide by driver datasheet directly or estimated from the testing conditions, i.e. RHOH=VOHH/IHO;
  • RGate – External gate drive resistance;
  • R(GFET_Int) – MOSFET internal gate resistance, provided by transistor datasheet;

Similarly, Peak HO pull-down current is shown in Equation 8.

Equation 8. LM5109B-Q1 eq06_snvsag6.gif

where

  • RHOL is HO pull-down resistance

Peak LO pullup current is shown in Equation 9.

Equation 9. LM5109B-Q1 eq07_snvsag6.gif

where

  • RLOH is LO pull-up resistance.

Peak LO pulldown current is shown in Equation 10.

Equation 10. LM5109B-Q1 eq08_snvsag6.gif

where

  • RLOL is LO pull-down resistance

For some scenarios, if the applications require fast turn-off, an anti-paralleled diode on RGate could be used to bypass the external gate drive resistor and speed-up turn-off transition.

8.2.2.4 Estimate the Driver Power Loss

The total driver IC power dissipation can be estimated through the following components.

  1. Static power losses, PQC, due to quiescent current – IDD and IHB;
  2. Equation 11. PQC = VDD × IDD + (VDD – VDH) × IHB
  3. Level-shifter losses, PIHBS, due high side leakage current – IHBS;
  4. Equation 12. PIHBS = VHB × IHBS × D

    where

    • D is high side switch duty cycle
  5. Dynamic losses, PQG1&2, due to the FETs gate charge – QG;
  6. Equation 13. LM5109B-Q1 eq09_snvsag6.gif

    where

    • QG is total FETs gate charge;
    • fSW is switching frequency;
    • RGD_R is average value of pull-up and pull-down resistor;
    • RGate is external gate drive resistor;
    • RGFET_Int is internal FETs gate resistor;
  7. Level-shifter dynamic losses, PLS, during high side switching due to required level-shifter charge on each switching cycle – QP;
  8. Equation 14. PLS = VHB × QP × fSW

In this example, the estimated gate driver loss in LM5109B-Q1 is shown in Equation 15.

Equation 15. LM5109B-Q1 eq10_snvsag6.gif

For a given ambient temperature, the maximum allowable power loss of the IC can be defined as shown in Equation 16.

Equation 16. LM5109B-Q1 eq11_snvsag6.gif

where

  • PLM5109BQ = The total power dissipation of the driver
  • TJ = Junction temperature
  • TA = Ambient temperature
  • RθJA = Junction-to-ambient thermal resistance

The thermal metrics for the driver package is summarized in the Thermal Information section of the datasheet. For detailed information regarding the thermal information table, please refer to the Texas Instruments application note entitled Semiconductor and IC Package Thermal Metrics (SPRA953.).

8.2.3 Application Curves

Figure 15 and Figure 16 shows the rising/falling time and turn-on/off propagation delay testing waveform in room temperature, and waveform measurement data (see the bottom part of the waveform). Each channel, HI/LI/HO/LO, is labeled and displayed on the left hand of the waveforms.

The testing condition: load capacitance is 1 nF, VDD = 12 V, fSW = 500 kHz.

HI and LI share one same input from function generator, therefore, besides the propagation delay and rising/falling time, the difference of the propagation delay between HO and LO gives the propagation delay matching data.

LM5109B-Q1 wvfm01_rising_time_turn_on_snvsag6.gif
CL = 1 nF VDD = 12 V fSW = 500 kHz
Figure 15. Rising Time and Turn-On Propagation Delay
LM5109B-Q1 wvfm02_falling_time_turn_off_snvsag6.gif
CL = 1 nF VDD = 12 V fSW = 500 kHz
Figure 16. Falling Time and Turn-Off Propagation Delay