SNVS653E July 2011 – August 2015 LM3532
PRODUCTION DATA.
The LM3532 contains an inductive boost converter which sees a high switched voltage (up to 40 V) at the SW pin, and a step current (up to 1 A) through the Schottky diode and output capacitor each switching cycle. The high switching voltage can create interference into nearby nodes due to electric field coupling (I = CdV/dt). The large step current through the diode, and the output capacitor can cause a large voltage spike at the SW pin and the OVP pin due to parasitic inductance in the step current conducting path (V = LdI/dt). Board layout guidelines are geared towards minimizing this electric field coupling and conducted noise. Figure 44 highlights these two noise generating components.
Figure 44. LM3532'S Boost Converter Showing Pulsed Voltage at SW (High Dv/Dt) and The following lists the main (layout sensitive) areas of the LM3532 in order of decreasing importance:
Output Capacitor
Schottky Diode
Inductor
Input Capacitor
The output capacitor is in the path of the inductor current discharge current. As a result, COUT sees a high current step from 0 to IPEAK each time the switch turns off and the Schottky diode turns on. Typical turnoff/turnon times are around 5 ns. Any inductance along this series path from the cathode of the diode through COUT and back into the LM3532's GND pin contributes to voltage spikes (VSPIKE = LPX × dI/dt) at SW and OUT which can potentially over-voltage the SW pin, or feed through to GND. To avoid this, COUT+ must be connected as close as possible to the Cathode of the Schottky diode and COUT− must be connected as close as possible to the LM3532's GND bump. The best placement for COUT is on the same layer as the LM3532 to avoid any vias that add extra series inductance (see Layout Examples).
The Schottky diode is in the path of the inductor current discharge. As a result the Schottky diode sees a high current step from 0 to IPEAK each time the switch turns off and the diode turns on. Any inductance in series with the diode causes a voltage spike (VSPIKE = LPX × dI/dt) at SW and OUT which can potentially over-voltage the SW pin, or feed through to VOUT and through the output capacitor and into GND. Connecting the anode of the diode as close as possible to the SW pin and the cathode of the diode as close as possible to COUT+ reduces the inductance (LPX) and minimize these voltage spikes (see Layout Examples).
The node where the inductor connects to the LM3532’s SW bump has 2 issues. First, a large switched voltage (0 to VOUT + VF_SCHOTTKY) appears on this node every switching cycle. This switched voltage can be capacitively coupled into nearby nodes. Second, there is a relatively large current (input current) on the traces connecting the input supply to the inductor and connecting the inductor to the SW bump. Any resistance in this path can cause large voltage drops that negatively affect efficiency.
To reduce the capacitively coupled signal from SW into nearby traces, the SW bump to inductor connection must be minimized in area. This limits the PCB capacitance from SW to other traces. Additionally, other nodes need to be routed away from SW and not directly beneath. This is especially true for high impedance nodes that are more susceptible to capacitive coupling such as (SCL, SDA, HWEN, PWM, and possibly ASL1 and ALS2). A GND plane placed directly below SW helps isolate SW and dramatically reduce the capacitance from SW into nearby traces.
To limit the trace resistance of the VBATT to inductor connection and from the inductor to SW connection, use short, wide traces (see Layout Examples).
The input bypass capacitor filters the inductor current ripple, and the internal MOSFET driver currents during turn on of the power switch.
The driver current requirement can be a few hundred milliamps with 5 ns rise and fall times. This appears as high dI/dt current pulses coming from the input capacitor each time the switch turns on. Close placement of the input capacitor to the IN pin and to the GND pin is critical because any series inductance between IN and CIN+ or CIN− and GND can create voltage spikes that could appear on the VIN supply line and in the GND plane.
Close placement of the input bypass capacitor at the input side of the inductor is also critical. The source impedance (inductance and resistance) from the input supply, along with the input capacitor of the LM3532, form a series RLC circuit. If the output resistance from the source (RS) is low enough the circuit is underdamped and has a resonant frequency (typically the case). Depending on the size of LS the resonant frequency could occur below, close to, or above the LM3532's switching frequency. This can cause the supply current ripple to be:
Figure 45 shows this series RLC circuit formed from the output impedance of the supply and the input capacitor. The circuit is re-drawn for the AC case where the VIN supply is replaced with a short to GND and the LM3532 + Inductor is replaced with a current source (ΔIL).
Equation 1 is the criteria for an underdamped response. Equation 2 is the resonant frequency. Equation 3 is the approximated supply current ripple as a function of LS, RS, and CIN.
As an example, consider a 3.6-V supply with 0.1 Ω of series resistance connected to CIN through 50 nH of connecting traces. This results in an underdamped input filter circuit with a resonant frequency of 712 kHz. Because the switching frequency lies near to the resonant frequency of the input RLC network, the supply current is probably larger then the inductor current ripple. In this case, using equation 3 from Figure 45, the supply current ripple can be approximated as 1.68 times the inductor current ripple. Increasing the series inductance (LS) to 500 nH causes the resonant frequency to move to around 225 kHz and the supply current ripple to be approximately 0.25 times the inductor current ripple.
Figure 45. Input RLC Network