ZHCSIM4H April   2009  – November 2014 LM25011 , LM25011-Q1

PRODUCTION DATA.  

  1. 特性
  2. 应用
  3. 说明
    1.     典型应用
  4. 修订历史记录
  5. Pin Configuration and Functions
    1.     Pin Functions
  6. Specifications
    1. 6.1 Absolute Maximum Ratings
    2. 6.2 Handling Ratings: LM25011
    3. 6.3 Handling Ratings: LM25011-Q1
    4. 6.4 Recommended Operating Conditions
    5. 6.5 Thermal Information
    6. 6.6 Electrical Characteristics
    7. 6.7 Typical Characteristics
  7. Detailed Description
    1. 7.1 Overview
    2. 7.2 Functional Block Diagram
    3. 7.3 Feature Description
      1. 7.3.1 Control Circuit Overview
      2. 7.3.2 On-Time Timer
      3. 7.3.3 Current Limit
      4. 7.3.4 Ripple Requirements
      5. 7.3.5 N-Channel Buck Switch and Driver
      6. 7.3.6 Soft-Start
      7. 7.3.7 Power Good Output (PGD)
      8. 7.3.8 Thermal Shutdown
    4. 7.4 Device Functional Modes
      1. 7.4.1 Shutdown Function
  8. Application and Implementation
    1. 8.1 Application Information
    2. 8.2 Typical Application
      1. 8.2.1 LM25011 Example Circuit
        1. 8.2.1.1 Design Requirements
        2. 8.2.1.2 Detailed Design Procedure
          1. 8.2.1.2.1 Custom Design with WEBENCH Tools
          2. 8.2.1.2.2 External Components
        3. 8.2.1.3 Application Curves
      2. 8.2.2 Output Ripple Control
        1. 8.2.2.1 Option A: Lowest Cost Configuration
        2. 8.2.2.2 Option B: Intermediate VOUT Ripple Configuration
        3. 8.2.2.3 Option C: Minimum VOUT Ripple Configuration
  9. Power Supply Recommendations
  10. 10Layout
    1. 10.1 Layout Guidelines
    2. 10.2 Layout Example
    3. 10.3 Power Dissipation
  11. 11器件和文档支持
    1. 11.1 使用 WEBENCH 工具创建定制设计
    2. 11.2 接收文档更新通知
    3. 11.3 相关链接
    4. 11.4 商标
    5. 11.5 静电放电警告
    6. 11.6 术语表
  12. 12机械、封装和可订购信息

封装选项

机械数据 (封装 | 引脚)
散热焊盘机械数据 (封装 | 引脚)
订购信息

External Components

The procedure for calculating the external components is illustrated with a design example using the LM25011. Referring to the Functional Block Diagram, the circuit is to be configured for the following specifications:

  • VOUT = 5 V
  • VIN = 8 V to 36 V
  • Minimum load current for continuous conduction mode IOUT(min) = 300 mA
  • Maximum load current IOUT(max) = 1.5 A
  • Switching frequency (FSW) = 1.0 MHz
  • Soft-start time = 5 ms

RFB2 and RFB1: These resistors set the output voltage, and their ratio is calculated from:

Equation 8. RFB2/RFB1 = (VOUT / 2.51 V) – 1

For this example, RFB2/RFB1 = 0.992. RFB1 and RFB2 should be chosen from standard value resistors in the range of 1.0 kΩ to 10 kΩ which satisfy the above ratio. For this example, 4.99 kΩ is chosen for both resistors, providing a 5.02-V output.

RT: This resistor sets the on-time and (by default) the switching frequency. First check that the desired frequency does not require an on-time or off-time shorter than the minimum allowed values (90 ns and 150, respectively). The minimum on-time occurs at the maximum input voltage. For this example:

Equation 9. LM25011 LM25011-Q1 LM25011A LM25011A-Q1 30094627.gif

The minimum off-time occurs at the minimum input voltage. For this example:

Equation 10. LM25011 LM25011-Q1 LM25011A LM25011A-Q1 30094628.gif

Both the on-time and off-time are acceptable because they are significantly greater than the minimum value for each. The RT resistor is calculated from Equation 6 using the minimum input voltage:

Equation 11. LM25011 LM25011-Q1 LM25011A LM25011A-Q1 30094629.gif

A standard value 118-kΩ resistor is selected. The minimum on-time calculates to 152 ns at VIN = 36 V, and the maximum on-time calculates to 672 ns at VIN = 8 V.

L1: The parameters controlled by the inductor are the inductor current ripple amplitude (IOR), and the ripple voltage amplitude across the current sense resistor RS. The minimum load current is used to determine the maximum allowable ripple to maintain continuous conduction mode (the lower peak does not reach 0 mA). This is not a requirement of the LM25011, but serves as a guideline for selecting L1. For this example, the maximum ripple current should be less than:

Equation 12. IOR(max) = 2 × IOUT(min) = 600 mAP-P

For applications where the minimum load current is zero, a good starting point for allowable ripple is 20% of the maximum load current. In this case substitute 20% of IOUT(max) for IOUT(min) in Equation 12. The ripple amplitude calculated in Equation 12 is then used in Equation 13:

Equation 13. LM25011 LM25011-Q1 LM25011A LM25011A-Q1 30094630.gif

A standard value 10-µH inductor is chosen. Using this inductor value, the maximum ripple current amplitude, which occurs at maximum VIN, calculates to 472 mAP-P, and the peak current is 1736 mA at maximum load current. Ensure the selected inductor is rated for this peak current. The minimum ripple current, which occurs at minimum VIN, calculates to 200 mAP-P.

RS: The minimum current limit threshold is calculated at maximum load current using the minimum ripple current calculated above. The current limit threshold is the lower peak of the inductor current waveform when in current limit (see Figure 15).

Equation 14. ILIM = 1.5 A – (0.2 A / 2) = 1.4 A

Current limit detection occurs when the voltage across the sense resistor (RS) reaches the current limit threshold. To allow for tolerances, the sense resistor value is calculated using the minimum threshold specification:

Equation 15. RS = 115 mV / 1.4 A = 82 mΩ

The next smaller standard value, 80 mΩ, is selected. The next step is to ensure that sufficient ripple voltage occurs across RS with this value sense resistor. As mentioned in the Ripple Requirements section, a minimum of 15-mVP-P voltage ripple is required across the RS sense resistor during the off-time to ensure the regulation circuit operates properly. The ripple voltage is the product of the inductor ripple current amplitude and the sense resistor value. In this case, the minimum ripple voltage calculates to:

Equation 16. VRIPPLE = ΔI × RS = 200 mA × 0.080 Ω = 16 mV

If the ripple voltage had calculated to less than 15 mVP-P, the inductor value would have to be reduced to increase the ripple current amplitude. This would have required a recalculation of ILIM and RS in the above equations. Because the minimum requirement is satisfied in this case, no change is necessary.

The nominal current limit threshold calculates to 1.63 A. The minimum and maximum thresholds calculate to 1.44 A and 1.83 A, respectively, using the minimum and maximum limits for the current limit threshold specification. The load current is equal to the threshold current plus one-half of the ripple current. Under normal load conditions, the maximum power dissipation in RS occurs at maximum load current, and at maximum input voltage where the on-time duty cycle is minimum. In this design example, the minimum on-time duty cycle is:

Equation 17. LM25011 LM25011-Q1 LM25011A LM25011A-Q1 30094631.gif

At maximum load current, the power dissipation in RS is equal to:

Equation 18. P(RS) = (1.5 A)2 × 0.080 Ω × (1 – 0.139) = 155 mW

When in current limit the maximum power dissipation in RS calculates to

Equation 19. P(RS) = (1.83 A + 0.472 A / 4)2 × 0.080 Ω = 304 mW

Duty cycle is not included in this power calculation because the on-time duty cycle is typically <5% when in current limit.

COUT: The output capacitor should typically be no smaller than 3.3 µF, although that is dependent on the frequency and the desired output characteristics. COUT should be a low ESR good-quality ceramic capacitor. Experimentation is usually necessary to determine the minimum value for COUT, as the nature of the load may require a larger value. A load which creates significant transients requires a larger value for COUT than a non-varying load.

CIN and CBYP: The purpose of CIN is to supply most of the switch current during the on-time, and limit the voltage ripple at VIN, because it is assumed the voltage source feeding VIN has some amount of source impedance. When the buck switch turns on, the current into VIN suddenly increases to the lower peak of the inductor ripple current, then ramps up to the upper peak, and finally drops to zero at turn-off. The average current during the on-time is the average load current. For a worst case calculation, CIN must supply this average load current during the maximum on-time, without letting the voltage at the VIN pin drop below a minimum operating level of 5.5 V. For this exercise 0.5 V is chosen as the maximum allowed input ripple voltage. Using the maximum load current, the minimum value for CIN is calculated from:

Equation 20. LM25011 LM25011-Q1 LM25011A LM25011A-Q1 30094632.gif

where tON is the maximum on-time, and ΔV is the allowable ripple voltage at VIN. The purpose of CBYP is to minimize transients and ringing due to long lead inductance leading to the VIN pin. A low ESR 0.1-µF ceramic chip capacitor is recommended, and CBYP must be located close to the VIN and SGND pins.

CBST: The recommended value for CBST is 0.1 µF. A high-quality ceramic capacitor with low ESR is recommended as CBST supplies a surge current to charge the buck switch gate at each turn-on. A low ESR also helps ensure a complete recharge during each off-time.

CSS: The capacitor at the SS pin determines the soft-start time, that is, the time for the output voltage to reach its final value (t1 in Figure 17). For a soft-start time of 5 ms, the capacitor value is determined from the following:

Equation 21. LM25011 LM25011-Q1 LM25011A LM25011A-Q1 30094633.gif

D1: A Schottky diode is recommended. Ultra-fast recovery diodes are not recommended as the high-speed transitions at the SW pin may affect the regulator operation due to the reverse recovery transients of the diode. The diode must be rated for the maximum input voltage, the maximum load current, and the peak current which occurs when the current limit and maximum ripple current are reached simultaneously. The average power dissipation of the diode is calculated from:

Equation 22. PD1 = VF × IOUT × (1 – D)

where VF is the forward voltage drop of the diode, and D is the on-time duty cycle.