ZHCSKH8C December 2009 – December 2019 BQ24072T , BQ24075T , BQ24079T
PRODUCTION DATA.
The BQ2407xT devices contain internal safety timers for the pre-charge and fast-charge phases to prevent potential damage to the battery and the system. The timers begin at the start of the respective charge cycles. The timer values are programmed by connecting a resistor from TMR to VSS. The resistor value is calculated using the following equation:
tPRECHG = KTMR × RTMR
tMAXCHG = 10 × KTMR × RTMR
Leave TMR unconnected to select the internal default timers. Disable the timers by connecting TMR to VSS.
Note that timers are suspended when the device is in thermal shutdown, and the timers are slowed proportionally to the charge current when the device enters thermal regulation.
During each of these events, the internal timers are slowed down proportionately to the reduction in charging current. For example, if the charging current is reduced by half for two minutes, the timer clock is reduced to half the frequency and the counter counts half as fast resulting in only one minute of "counting" time.
If the precharge timer expires before the battery voltage reaches VLOWV, the BQ2407xT indicates a fault condition. Additionally, if the battery current does not fall to ITERM before the fast charge timer expires, a fault is indicated. The CHG output flashes at approximately 2 Hz to indicate a fault condition. The fault condition is cleared by toggling CE or the input power, entering/ exiting USB suspend mode, or an OVP event.