ZHCSRG2G May 2001 – December 2022 BQ2057C , BQ2057W
PRODUCTION DATA
The BQ2057 continuously monitors temperature by measuring the voltage between the TS and VSS pins. A negative- or a positive-temperature coefficient thermistor (NTC, PTC) and an external voltage divider typically develop this voltage. (See Figure 10-9.) The BQ2057 compares this voltage against its internal V(TS1) and V(TS2) thresholds to determine if charging is allowed. (See Figure 10-10.) The temperature sensing circuit is immune to any fluctuation in VCC, since both the external voltage divider and the internal thresholds (V(TS1) and V(TS2)) are referenced to VCC.
The resistor values of R(T1) and R(T2) are calculated by the following equations:
For NTC Thermistors


For PTC Thermistors


Where R(TC) is the cold temperature resistance and R(TH) is the hot temperature resistance of thermistor, as specified by the thermistor manufacturer.
RT1 or RT2 can be omitted If only one temperature (hot or cold) setting is required. Applying a voltage between the V(TS1) and V(TS2) thresholds to pin TS disables the temperature-sensing feature.
Figure 10-9 Temperature Sensing Circuits
Figure 10-10 BQ2057 TS
Input Thresholds