ZHCSM49 April 2021 AMC3336-Q1
PRODUCTION DATA
Do not leave the inputs of the AMC3336-Q1 unconnected (floating) when the device is powered up. If both modulator inputs are left floating, the modulator outputs a bitstream that is undefined.
Connect the high-side ground (HGND) to INN, either directly or through a resistive path. A DC current path between INN and HGND is required to define the input common-mode voltage. Take care not to exceed the input common-mode range, as specified in the Section 6.3 table.
The high-side LDO can source a limited amount of current (IH) to power external circuitry. Take care not to over-load the high-side LDO and be aware of the drating of IH at high temperatures as explined in the Section 7.3.5 section.
The low-side LDO does not output a constant voltage and is not intended for powering any external circuitry. Do not connect any external load to the HLDO_OUT pin.