ZHCSIK6D November 2017 – June 2024 ADS8166 , ADS8167 , ADS8168
PRODUCTION DATA
Figure 6-1 shows the small-signal equivalent circuit of the sample-and-hold circuit. Each sampling switch is represented by resistance (RS1 and RS2, typically 50Ω) in series with an ideal switch (SW). The sampling capacitors, CS1 and CS2, are typically 60pF.
The multiplexer on-resistance (RMUX), is typically a 40Ω resistor in series between the ON channel and the MUXOUT-P or MUXOUT-M pins. The multiplexer analog input typically has a 13pF on-channel capacitance (CMUX).
Figure 6-1 Input Sampling Stage Equivalent CircuitDuring the input signal acquisition phase, the ADC-INP and ADC-INM inputs are individually sampled on CS1 and CS2, respectively. During the conversion process, the device converts for the voltage difference between the two sampled values: VADC-INP – VADC-INM.
Each analog input pin has electrostatic discharge (ESD) protection diodes to AVDD and GND. Keep the analog inputs within the specified range to avoid turning the diodes on.