SLAS468A June 2005 – August 2016 ADS7887 , ADS7888
PRODUCTION DATA.
The reference voltage for the ADS7887 and ADS7888 A/D converters are derived from the supply voltage internally. The supply to these converters must be driven with a low impedance source and must be decoupled to the ground Decouple the VDD with 1-µF ceramic decoupling capacitors, as shown in Figure 40. Always set the VDD supply to be greater than or equal to the maximum input signal to avoid saturation of codes.
Figure 40. Supply and Reference Decoupling Capacitors
Figure 41. Using the REF3030 Reference
Figure 42. Buffering With the OPA735