TIDUF06 August 2022
One of the most critical portions of a design that uses POC is the filter circuitry. The goal is twofold:
The DS90UB953-Q1 and DS90UB960-Q1 SerDes devices used in this system communicate over two carrier frequencies, 2 GHz at full speed ("forward channel") and a lower frequency of 50 MHz ("backchannel") determined by the deserializer device. The filter must attenuate this rather large band spanning both carriers, hoping to pass only DC. To allow the forward channel and backchannel to pass uninterrupted over the POC cable, an impedance of > 2 kΩ across the 25-MHz to 2-GHz bandwidth is required. To accomplish this, an inductor is typically chosen for filtering the 25-MHz to 1-GHz range, while a ferrite bead is chosen for filtering the 1- to 2-GHz frequency band. This complete filter is shown by L2 in Figure 2-8. L1 is the same inductor for the POC filter on the deserializer side. In this camera design, it is imperative for the filter to have the smallest footprint allowable. To accomplish this, the LQH3NPZ100MJRL 10-µH inductor is chosen because it has a wide band impedance that filters from 10 MHz to 1 GHz. This eliminates the need for a solution that would typically require two inductors, one for the lower frequency and another for the higher frequency.
For the high-frequency forward-channel filtering, this reference design uses three 1.5-kΩ ferrite beads in series with the 10-µH inductor to bring the impedance above 2 kΩ across the 1- to 2-GHz range. This design uses three 1.5-kΩ ferrite beads because when in operation, the current through these devices reduces the effective impedance. Therefore, three ferrite beads instead of two allows for more headroom across the whole frequency band. For good measure, this design uses a 4-kΩ resistor in parallel with the 10-µH inductor to provide a constant impedance across the complete frequency band for impedance smoothing. With this approach, the solution size can be minimized onboard for the POC inductor filtering. For more details, see the Power-over-Coax Design Guidelines for DS90UB953-Q1 application report.
Lastly, in regards to filtering, ensuring that the FPD-Link signal is uninterrupted is just as important as providing a clean, noise-free DC supply to the system. To achieve this, AC coupling capacitors of 0.033 µF and 0.015 µF are chosen to ensure the high-speed AC data signals are passed through, but the DC is blocked from getting on the data lines.