SWRZ129B september   2022  – june 2023 CC2674R10

PRODUCTION DATA  

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Advisories Matrix
  5. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development Support-Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  6. 3Advisories
    1.     Radio_01
    2. 3.1 Radio_05
    3.     Power_03
    4.     PKA_01
    5.     PKA_02
    6.     I2C_01
    7.     I2S_01
    8.     CPU_Sys_01
    9.     Sys_01
    10. 3.2 Sys_06
    11.     SYSCTRL_01
    12.     IOC_01
    13.     ADC_02
  7. 4Revision History

I2S_01

I2S Bus Faults are Not Reported

Revisions Affected:

Revision B

Details:

The I2S module will not set the bus error interrupt flag (I2S0.IRQFLAGS.BUS_ERR) if an I2S read or write causes a system bus fault that results from access to illegal addresses (usage error).

Workaround:

Software must ensure that memory area used by the I2S DMA is accessible, meaning that the memory is powered on and the system bus is connected..

As an example; The TI-provided SPI driver SPICC26X2DMA.c will ensure that the flash memory is kept accessible also in Idle power mode if the transmit buffer address starts with 0x0 to ensure no bus faults occur. A similar approach needs to be taken if writing a peripheral driver utilizing I2S.