SWRZ076D July   2018  – December 2020 CC1352P

 

  1.   1
  2.   2
  3.   3
    1.     4
    2.     5
    3.     6
  4.   7
    1.     8
    2.     9
    3.     10
    4.     11
    5.     12
    6.     13
    7.     14
    8.     15
    9.     16
    10.     17
    11.     18
    12.     19
    13.     20
    14.     21
    15.     22
    16.     23
    17.     24
    18.     25
    19.     26
    20.     27
    21.     28
  5.   29

ADC_05

Writing any value to AUX_ANAIF:ADCTRIG.START will create an ADC trigger

Revisions Affected:

Revision E and earlier

Details:

The original register documentation states that you need to write a ‘1’ to AUX_ANAIF:ADCTRIG.START to manually trigger the ADC. This is not correct, as any write will do this.

Workaround:

Avoid writing to AUX_ANAIF:ADCTRIG.START unless an ADC trigger should be generated.