SPRZ455D december 2020 – june 2023 DRA829J , DRA829J-Q1 , DRA829V , TDA4VM , TDA4VM-Q1
ADVANCE INFORMATION
PCIe: End of Interrupt (EOI) Not Enabled for PCIe Legacy Interrupts
A PCIe End Point (EP) can signal a legacy interrupt at the PCIe Root Port (RP) by issuing an ASSERT_INTx/DEASSERT_INTx message. The ASSERT_INTx message causes a level output signal at the boundary of the PCIe RP controller to go high and the DEASSERT_INTx message causes the same output signal to go low. This level output signal from the controller is converted to a pulse for signaling an interrupt to the SoC interrupt controller.
The EP can issue a single ASSERT_INTx message and maintain the level output of the RP controller high without issuing a DEASSERT_INTx message if there is pending work to be done. The End of Interrupt (EOI) feature in the interrupt logic is used to re-trigger the pulse interrupt to the SoC interrupt controller from a level signal that remains asserted. The EOI feature has not been enabled for the PCIe legacy interrupts. This will result in only a single pulse interrupt to be generated to the SoC interrupt controller even if the level output signal from the PCIe RP remains asserted high.
As a result of this issue, legacy interrupt in RP mode cannot be used if EPs attached to this RP cannot guarantee DEASSERT_INTx message for each interrupt event.
PCIe EP can use MSI/MSI-X to signal interrupts to the PCIe RP in lieu of legacy interrupts.