SPRZ455D december 2020 – june 2023 DRA829J , DRA829J-Q1 , DRA829V , TDA4VM , TDA4VM-Q1
ADVANCE INFORMATION
STOG: Error miscounting when there are two concurrent timeouts or two concurrent unexpected responses
When there is a read command and write command that timeout in the same cycle, the timeout counter will only increment by 1 instead of 2 in this situation. Likewise, if an unexpected read response and an unexpected write response both arrive in the same cycle, the unexpected response counter will only increment by 1 instead of 2.
The error counters are primarily supplemental information for software debug. Only one timeout error command/transaction info is recorded. The counters saturate at a count of 3, so the software should primarily focus on the error counter value being non-zero vs the exact counter value. The same approach should be applied to the unexpected response counter. Note: unexpected responses are dropped by the flush gasket.