• Menu
  • Product
  • Email
  • PDF
  • Order now
  • C2000 Software Frequency Response Analyzer (SFRA) Library and Compensation Designer in SDK Framework

    • SPRUIK4A September   2018  – June 2019 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S

       

  • CONTENTS
  • SEARCH
  • C2000 Software Frequency Response Analyzer (SFRA) Library and Compensation Designer in SDK Framework
  1.   C2000 Software Frequency Response Analyzer (SFRA) Library and Compensation Designer in SDK Framework
    1.     Trademarks
    2. 1 Introduction
    3. 2 Installing the SFRA Library
      1. 2.1 SFRA Library Package Contents
      2. 2.2 How to Install the SFRA Library
    4. 3 Module Summary
      1. 3.1 SFRA Library Function Summary
      2. 3.2 Principle of Operation
      3. 3.3 Per Unit Format
      4. 3.4 Floating Point (Singe Precision)
        1. 3.4.1 Object Definition
        2. 3.4.2 Module Interface Definition
        3. 3.4.3 Adding SFRA Library to the Project
        4. 3.4.4 Adding Support for SFRA GUI
      5. 3.5 Script for Importing Frequency Response and Designing Compensation
      6. 3.6 SFRA GUI Options and How to Run
    5. 4 Compensation Designer
      1. 4.1 Launching Compensation Designer
        1. 4.1.1 Standalone From SFRA GUI Folder
        2. 4.1.2 From Solution Adapter Page
      2. 4.2 Compensation Style and Number
    6. 5 Case Study
      1. 5.1 Plant TF Extraction
      2. 5.2 Designing Compensator Using Compensation Designer
      3. 5.3 OL Measurement
      4. 5.4 Comparing SFRA Measured Frequency Response Versus Modeled
    7. 6 Running Software Test Bench Example for SFRA
    8. 7 Using SFRA Without SFRA GUI Integration
    9. 8 FAQ
  2.   Revision History
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
USER'S GUIDE

C2000 Software Frequency Response Analyzer (SFRA) Library and Compensation Designer in SDK Framework

C2000™ Software Frequency Response Analyzer (SFRA) Library and Compensation Designer in SDK Framework

The Software Frequency Response Analyzer (SFRA) is a software library that enables developers to quickly measure the frequency response of their digital power converter. The SFRA library contains software functions that inject a frequency into the control loop and measure the response of the system using the C2000 MCUs’ on-chip analog to digital converter (ADC). This process provides the plant frequency response characteristics, the open loop gain frequency response and the closed loop frequency response of the closed loop system. This user's guide explains the software interface of the library and lists the steps needed to integrate the library into a project. The process to run the example project for the SFRA is also documented in this user's guide.

Trademarks

C2000, Code Composer Studio are registered trademarks of Texas Instruments.

All other trademarks are the property of their respective owners.

1 Introduction

Texas Instruments' software frequency response analyzer (SFRA) library is designed to enable frequency response analysis on digitally controlled power converters using software only and without the need for an external frequency response analyzer. The optimized library can be used in high frequency power conversion applications to identify the plant, the closed loop and the open loop gain characteristics of a closed loop power converter, which can be used to get stability information such as gain margin, phase margin and open loop gain crossover frequency, to evaluate the control loop performance.

NOTE

This documentation pertains to the SFRA Library released in the C2000WARE-DIGITALPOWER-SDK framework. At the time of authoring of this document, only the single precision floating point format of the library is available inside the SDK framework, the fixed-point version is not yet ported to the new software framework. For the fixed-point version of the library, see controlSUITE and the C2000™ Software Frequency Response Analyzer (SFRA) Library and Compensation Designer User's Guide.

Consider a digitally controlled closed loop power converter, as shown in Figure 1, where:

  • H is the transfer function of the plant that needs to be controlled
  • G is the digital compensator
  • GH is referred to as the open loop transfer function
  • CL is refrerred to as the closed loop transfer function and is GH/(1+GH)
  • r is the instantaneous set point or the reference of the converter
  • Ref is the DC set point reference
  • y the analog-to-digital converter (ADC) feedback
  • e the instantaneous error
  • d the sensor noise and disturbance
  • u the PWM duty cycle

The key objectives of the compensator in a closed loop system can be summarized as:

  • Ensure that the system is stable (for example, the system tracks the reference asymptotically)
  • Equation 1. eq1_spruhz5.gif
  • System provides disturbance rejection to ensure robust operation
  • Equation 2. eq2_spruhz5.gif
digit_contl_pwr_conv_spruhz5.gifFigure 1. Digitally Controlled Power Converter

Whether or not the system meets the objectives can be determined by knowing the open loop transfer function (GH), as shown in Equation 1 and Equation 2.

A Bode plot of the open loop transfer function GH is frequently used for this purpose and quantities such as gain margin (GM), phase margin (PM) and open loop gain crossover frequency (Folg_cf) are often used to comment on the stability and robustness of a closed loop power converter.

The closed loop transfer function (GH/(1+GH)) provides an idea of the tracking that is how good the system is able to track to the reference commanded.

The SFRA library can enable measurements of the GH, GH/(1+GH) and H frequency response by software. This data can be used to:

  • Verify the plant model (H) or extract the plant model (H)
  • Design a compensator (G) for the closed loop plant
  • Verify the close loop performance of the system by plotting the open loop (GH) or Closed Loop (GH/(1+GH)) Bode diagram

As the frequency response of GH and H carry information of the plant, the data can be used to comment on the health of the power stage by periodically measuring the frequency response.

The SFRA library is based on sinusoidal injection principle, where the assumption is that the injection amplitude causes very small deviation to the normal operating point of the converter. The SFRA library can be integrated into the control code of the power converter, this document details the steps to do so. All computations for the GH, H and CL calculations are done on the MCU and the entire arrays of the GH, H and CL magnitude and phase response are stored on the controller. For visualization purpose, a GUI is also provided with the tool. This GUI can be used to start a frequency response sweep, observer progress of the SFRA sweep and analyze the GH, H and CL plots generated after the FRA sweeps.

Once integrated into the code, the SFRA library can be used to design or fine tune the controller. For this, a typical flow of using SFRA library is:

  1. Initiate a SFRA sweep in open loop through the SFRA GUI that populates the data in a comma separate value (CSV) file, stored at the location where SFRA GUI is invoked from. This information can then be used to identify the plant model for the steady state operating point at which the SFRA sweep has been conducted.
  2. NOTE

    Optionally, the SFRA GUI can output data to an excel file.

  3. This SFRA CSV data can directly be used in the Compensation Designer to design a compensator that meets the system requirements. (Alternatively, if the Excel file option was used from the GUI, the MATLAB script provided with this package can be used to read that data into MATLAB and then curve fit the response to a transfer function. Sisotool can then be used to design the compensator).
  4. New Compensator values can be copied from the compensation designer GUI or MATLAB into the Code Composer Studio™ project.
  5. Compile and load the code with new coefficients into the microcontroller controlling the power stage. SFRA algorithm (Step 1) can be re-run to verify the closed loop system performance by measuring the open loop gain GH (also referred to as loop gain in many literatures).

In summary, TI’s software frequency response analyzer along with the Compensation Designer provides a methodology to tune power supplies in a systematic way and enables quick and easy frequency response analysis for power converters without the need of external connections and equipment, as shown in Figure 2. Since no external connections are used, the SFRA can be run repeatedly to periodically assess the health of the power converter and get diagnostic information.

SW_SFRA_freq_resp_data2_spruhz5.gifFigure 2. Control Design Using SFRA Library and Compensation Designer

2 Installing the SFRA Library

2.1 SFRA Library Package Contents

The TI SFRA library consists of the following components:

  • Header files and software library for single precision floating-point computation
  • C2000 Software Frequency Response Analyzer (SFRA) Library User's Guide
  • SFRA Graphical User Interface to display the frequency response analysis results
  • Scripts to import SFRA data into MATLAB
  • Example software test bench project to quickly evaluate SFRA library

2.2 How to Install the SFRA Library

The SFRA library is distributed through the C2000WARE-DIGITALPOWER-SDK installer, which can be downloaded at http://www.ti.com/tool/C2000WARE-DIGITALPOWER-SDK , alternatively it may be available as part of other SDKs for C2000 MCUs that use SFRA library. By default, the installation places the library components in the following directory structure:

C:\ti\c2000\C2000Ware_DigitalPower_SDK_<version>\libraries\sfra

The following sub-directory structure is shown in Table 1.

Table 1. Library Sub-Directory Structure

<base>\docs Documentation
<base>\examples Contains example projects for quickly evaluating SFRA (Software Test Bench). Currently one example inclued is example1_stb which is a software check for the SFRA library.
<base>\gui Host side graphical user interface (SFRA_GUI.exe) that is used for displaying the frequency response and the GUI tool Compensation Designer (ComDesigner.exe) that can be used to design compensator based with the SFRA measured plant information. The SFRAData.csv file is also stored here.
<base>\include Contains the header file that is needed to be included in the system project to use this libarary.
<base>\lib The library file for float32 and float32+TMU processor options.
<base>\scripts Scripts to import SFRA data for compensation design in MATLAB.
<base> Software manifest with version number of the library.

3 Module Summary

3.1 SFRA Library Function Summary

The SFRA library consists of modules that enable the user to run SFRA on power converters. Table 2 lists the modules existing in the SFRA library and a summary of cycle counts on each instruction set variant of the SFRA library.

Table 2. SFRA Cycle and Program Memory Usage

SFRA_INJECT SFRA_COLLECT SFRA_Background Program Size Data Size
Float 41 71 Typical ~ 50
Max 2350
1109 x 16-bit words 22 x 16-bit words (internal) + 31 x 16-bit words for SFRA object
Float TMU 37 67 Typical ~50
Max 407
1098 x 16-bit words 22 x 16-bit words (internal) + 31 x 16-bit words for SFRA object

The numbers reported above are for the data memory usage internal to the library and the memory used by the SFRA object instance. The memory used to store the frequency response data is not included as this is user specific, and depend on the number of frequency points the user wants to run the SFRA over. The number for inject and collect routine are reported for when active sweep is in progress and are the worst case. If no sweep in progress the routines take significnatly less cycles.

NOTE

  • The SFRA library is non-re-entrant (only one instance of the SFRA library is supported in a particular project).
  • The cycles reported, unless otherwise mentioned, are for maximum/worst case path in the operation. The cycles reported include the branch to the routine and return to the next instruction after the branch. Cycles taken to push parameters on the stack before the branch are not accounted for in this number as it can vary depending on adjoining code in the program.
  • For the floating-point library, the memory for RTS library calls that execute trigonometric operations is not included.
  • TMU provides additional acceleration that improves performance in the background loops.

 

Texas Instruments

© Copyright 1995-2025 Texas Instruments Incorporated. All rights reserved.
Submit documentation feedback | IMPORTANT NOTICE | Trademarks | Privacy policy | Cookie policy | Terms of use | Terms of sale