SFFS119 March   2021 TS5A23157-Q1

 

  1.   1
  2.   2
  3.   3
  4.   4
  5.   5

Pin Failure Mode Analysis (Pin FMA)

This section provides a Failure Mode Analysis (FMA) for the pins of the TS5A23157-Q1. The failure modes covered in this document include the typical pin-by-pin failure scenarios:

  • Pin short-circuited to Ground (see Table 4-2)
  • Pin open-circuited (see Table 4-3)
  • Pin short-circuited to an adjacent pin (see Table 4-4)
  • Pin short-circuited to supply (see Table 4-5)

Table 4-2 through Table 4-5 also indicate how these pin conditions can affect the device as per the failure effects classification in Table 4-1.

Table 4-1 TI Classification of Failure Effects
Class Failure Effects
A Potential device damage that affects functionality
B No device damage, but loss of functionality
C No device damage, but performance degradation
D No device damage, no impact to functionality or performance

Figure 4-1 shows the TS5A23157-Q1 pin diagram. For a detailed description of the device pins please refer to the Pin Configuration and Functions section in the TS5A23157-Q1 data sheet.

GUID-8D4826FC-0A3A-4FF2-A519-0C8E8D9C0350-low.gif Figure 4-1 Pin Diagram
Table 4-2 Pin FMA for Device Pins Short-Circuited to Ground
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class

IN1

1

IN stuck low. Cannot control switch states.

B

NO1

2

Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

GND

3

No effect, normal operation.

D

NO2

4

Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

IN2

5

IN stuck low. Cannot control switch states.

B

COM2

6

Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

NC2

7

Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

V+

8

Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible.

A

NC1

9

Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

COM1

10

Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

Table 4-3 Pin FMA for Device Pins Open-Circuited
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
IN1 1 Loss of control of IN pin. Switch in undefined state.

B

NO1 2 Corruption of analog signal.

B

GND 3 Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible.

A

NO2 4 Corruption of analog signal.

B

IN2 5 Loss of control of IN pin. Switch in undefined state.

B

COM2 6 Corruption of analog signal.

B

NC2 7 Corruption of analog signal.

B

V+ 8 Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible.

A

NC1 9 Corruption of analog signal.

B

COM1 10 Corruption of analog signal.

B

Table 4-4 Pin FMA for Device Pins Short-Circuited to Adjacent Pin
Pin Name Pin No. Shorted to Description of Potential Failure Effect(s) Failure Effect Class
IN1 1 NO1 Loss of control of IN pin. Switch in undefined state. Possible corruption of analog signal.

B

NO1 2 COM1 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

COM1 3 NO2 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

NO2 4 IN2 Loss of control of IN pin. Switch in undefined state. Possible corruption of analog signal.

B

IN2 5 COM2 Not considered, Corner pin.

D

COM2 6 NC2 Corruption of analog signal.

B

NC2 7 V+ Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

V+ 8 NC1 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

NC1 9 COM1 Corruption of analog signal.

B

COM1 10 IN1 Not considered, Corner pin.

D

Table 4-5 Pin FMA for Device Pins Short-Circuited to VSSOP
Pin Name Pin No. Description of Potential Failure Effect(s) Failure Effect Class
IN1 1 IN stuck to VDD. Cannot control switch states.

B

NO1 2 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

COM1 3 Device unpowered. Device not functional. Observe that the absolute maximum ratings for all pins of the device are met, otherwise device damage is possible.

A

NO2 4 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

IN2 5 IN stuck to VDD. Cannot control switch states.

B

COM2 6 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

NC2 7 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible.

A

V+ 8 No effect, normal operation

D

NC1 9 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible

A

COM1 10 Corruption of analog signal. If there is no limiting resistor in the switch path device damage is possible

A