DLPU082B August 2021 – August 2022 DLPC7540
The controller has several pre-defined patterns that the user can select using TPG Pre-defined Pattern command. Use the DLP Composer tool to configure these pre-defined patterns the controller TPG block generates the pattern data. This option is useful for:
These are additional configuration commands specific to test patterns.
Command Name | Description |
---|---|
Set TPG Border | Set border around selected TPG, border width can be 0 – 20; and border color programmable (R,G,B) value in the range of 0 - 1023. |
Set TPG Resolution | Set the TPG pattern resolution. In case the resolution of the pattern is smaller than the display resolution of the DMD, controller will fill the area with pleasing color. |
Set TPG FrameRate | Configure TPG frame-rate between 30Hz – 120Hz. There is dependency of the TPG resolution wrt frame-rate; for example, in case of 4K resolution max frame-rate will be limited to 60Hz and in case of 1080p resolution max frame rate will be limited to 240Hz. |