ZHCSSO5A July 2023 – October 2023 TPS7H2140-SEP
PRODUCTION DATA
High-accuracy current sense is implemented in the TPS7H2140-SEP. It allows a better real-time monitoring effect and more-accurate diagnostics without further calibration.
The integrated current mirror sources a ratio of the load current as: 1 / KCS (where: KCS = 300). This mirrored current flows into the external current sense resistor to become a voltage signal. The current mirror is shared by the four channels. Channel selection is accomplished by using the multiplexer digital inputs (SEL and SEH). ICS can be calculated using Equation 1.
KCS is the ratio of the output current and the sense current (CS). It is a constant value across the temperature and supply voltage (IN). Each device is calibrated accurately during production, so post-calibration is not required. See Figure 8-2 for more details.
When a fault occurs, the CS pin also works as a fault report with a pullup voltage of VCS_FAULT. During a fault the maximum available current in CS is ICS_FAULT (15 mA). See Figure 8-3 for more details.
Use Equation 2 to calculate RCS.
Take the following points into consideration when calculating RCS.