ZHCSKD3A November 2019 – February 2021 TPS6521815
PRODUCTION DATA
The TPS6521815 can be reset by holding the PB pin low for more than 8 or 15 s, depending on the value of the TRST bit. All rails are shut down by the sequencer and all register values reset to their default values. Rails not controlled by the sequencer are shut down additionally. Note: the RESET function power-cycles the device and only temporarily shuts down the output rails. Resetting the device does not lead to an OFF state. If the PB_IN pin is kept low for an extended amount of time, the device continues to cycle between the ACTIVE and RESET state, entering the RESET every 8 or 15 s.
The device is also reset if a PGOOD or OTS fault occurs. The TPS6521815 remains in the RECOVERY state until the fault is removed, at which time it transitions back to the ACTIVE state.