ZHCS614G October 2011 – September 2022 TPS40422
PRODUCTION DATA
TON_DELAY: | ||
This parameter selects the delay from when the output is enabled until soft-start beings, as a multiple of the TON_RISE time. The default value is 0. Values can range from 0 to 7 in increments of 1. | ||
TOFF_DELAY: | ||
This parameter selects the delay from when the output is disabled until the output stops switching, as a multiple of the TON_RISE time. The default value is 0. Values can range from 0 to 7 in increments of 1. |