SLOS367E August   2003  – November 2015 TPA6211A1

PRODUCTION DATA.  

  1. Features
  2. Applications
  3. Description
  4. Revision History
  5. Device Comparison Table
  6. Pin Configuration and Functions
  7. Specifications
    1. 7.1 Absolute Maximum Ratings
    2. 7.2 ESD Ratings
    3. 7.3 Recommended Operation Conditions
    4. 7.4 Thermal Information
    5. 7.5 Electrical Characteristics
    6. 7.6 Operating Characteristics
    7. 7.7 Dissipation Ratings
    8. 7.8 Typical Characteristics
  8. Parameter Measurement Information
  9. Detailed Description
    1. 9.1 Overview
    2. 9.2 Functional Block Diagram
    3. 9.3 Feature Description
      1. 9.3.1 Fully Differential Amplifier Efficiency and Thermal Information
        1. 9.3.1.1 Advantages of Fully Differential Amplifiers
        2. 9.3.1.2 Differential Output Versus Single-Ended Output
    4. 9.4 Device Functional Modes
      1. 9.4.1 Shutdown Mode
  10. 10Application and Implementation
    1. 10.1 Application Information
    2. 10.2 Typical Application
      1. 10.2.1 Design Requirements
      2. 10.2.2 Detailed Design Procedure
        1. 10.2.2.1 Selecting Components
          1. 10.2.2.1.1 Resistors (RI)
          2. 10.2.2.1.2 Bypass Capacitor (CBYPASS) and Start-Up Time
          3. 10.2.2.1.3 Input Capacitor (CI)
          4. 10.2.2.1.4 Band-Pass Filter (Ra, Ca, and Ca)
            1. 10.2.2.1.4.1 Step 1: Low-Pass Filter
            2. 10.2.2.1.4.2 Step 2: High-Pass Filter
            3. 10.2.2.1.4.3 Step 3: Additional Low-Pass Filter
          5. 10.2.2.1.5 Decoupling Capacitor (CS)
          6. 10.2.2.1.6 Using Low-ESR Capacitors
      3. 10.2.3 Application Curves
    3. 10.3 System Examples
  11. 11Power Supply Recommendations
    1. 11.1 Power Supply Decoupling Capacitor
  12. 12Layout
    1. 12.1 Layout Guidelines
    2. 12.2 Layout Examples
  13. 13Device and Documentation Support
    1. 13.1 Device Support
      1. 13.1.1 Development Support
    2. 13.2 Documentation Support
      1. 13.2.1 Related Documentation
    3. 13.3 Community Resources
    4. 13.4 Trademarks
    5. 13.5 Electrostatic Discharge Caution
    6. 13.6 Glossary
  14. 14Mechanical, Packaging, and Orderable Information

封装选项

请参考 PDF 数据表获取器件具体的封装图。

机械数据 (封装 | 引脚)
  • DGN|8
  • DRB|8
散热焊盘机械数据 (封装 | 引脚)
订购信息

9 Detailed Description

9.1 Overview

The TPA6211A1 is a fully differential amplifier with differential inputs and outputs. The fully differential amplifier consists of a differential amplifier and a common- mode amplifier. The differential amplifier ensures that the amplifier outputs a differential voltage that is equal to the differential input times the gain. The common-mode feedback ensures that the common-mode voltage at the output is biased around VDD/2 regardless of the common- mode voltage at the input.

9.2 Functional Block Diagram

TPA6211A1 tpa6211a1_bkd.gif

9.3 Feature Description

9.3.1 Fully Differential Amplifier Efficiency and Thermal Information

Class-AB amplifiers are inefficient, primarily because of voltage drop across the output-stage transistors. The two components of this internal voltage drop are the headroom or dc voltage drop that varies inversely to output power, and the sinewave nature of the output. The total voltage drop can be calculated by subtracting the RMS value of the output voltage from VDD. The internal voltage drop multiplied by the average value of the supply current, IDD(avg), determines the internal power dissipation of the amplifier.

An easy-to-use equation to calculate efficiency starts out as being equal to the ratio of power from the power supply to the power delivered to the load. To accurately calculate the RMS and average values of power in the load and in the amplifier, the current and voltage waveform shapes must first be understood (see Figure 28).

TPA6211A1 ai_VLRMS_los367.gif Figure 28. Voltage and Current Waveforms for BTL Amplifiers

Although the voltages and currents for SE and BTL are sinusoidal in the load, currents from the supply are different between SE and BTL configurations. In an SE application the current waveform is a half-wave rectified shape, whereas in BTL it is a full-wave rectified waveform. This means RMS conversion factors are different. Keep in mind that for most of the waveform both the push and pull transistors are not on at the same time, which supports the fact that each amplifier in the BTL device only draws current from the supply for half the waveform. The following equations are the basis for calculating amplifier efficiency.

These definitions are true for the following equations:

  • ηBTL = Efficiency of a BTL amplifier
  • PL = Power delivered to load
  • PSUP = Power drawn from power supply
  • VLRMS = RMS voltage on BTL load
  • VP = Peak voltage on BTL load
  • VDD = Power supply voltage
  • IDDavg = Average current drawn from the power supply

Use Equation 1 to calculate the efficiency of a BTL amplifier.

Equation 1. TPA6211A1 Q14a_slos367.gif

where

  • TPA6211A1 Q14b_slos367.gif

      where

    • TPA6211A1 Q14c_slos367.gif
    • therefore

    • TPA6211A1 Q14d_slos367.gif
  • TPA6211A1 Q14e_slos367.gif

      where

    • TPA6211A1 Q14f_slos367.gif
    • therefore

    • TPA6211A1 Q14g_slos367.gif

Using these values, substitute PL and PSUP from Equation 1 as shown in Equation 2.

Equation 2. TPA6211A1 Q14h_slos367.gif

where

  • TPA6211A1 Q14i_slos367.gif

Therefore, ηBTL can be calculated using Equation 3.

Equation 3. TPA6211A1 Q15_los367.gif

Table 2. Efficiency and Maximum Ambient Temperature vs Output Power

OUTPUT POWER
(W)
EFFICIENCY
(%)
INTERNAL DISSIPATION
(W)
POWER FROM SUPPLY
(W)
MAX AMBIENT TEMPERATURE (1)
(°C)
5-V, 3-Ω Systems
0.5 27.2 1.34 1.84 85(2)
1 38.4 1.6 2.6 76
2.45 60.2 1.62 4.07 75
3.1 67.7 1.48 4.58 82
5-V, 4-Ω BTL Systems
0.5 31.4 1.09 1.59 85(2)
1 44.4 1.25 2.25 85(2)
2 62.8 1.18 3.18 85(2)
2.8 74.3 0.97 3.77 85(2)
5-V, 8-Ω Systems
0.5 44.4 0.625 1.13 85(2)
1 62.8 0.592 1.6 85(2)
1.36 73.3 0.496 1.86 85(2)
1.7 81.9 0.375 2.08 85(2)
(1) DRB package
(2) Package limited to 85°C ambient

Table 2 uses Equation 3 to calculate efficiencies for four different output power levels. Note that the efficiency of the amplifier is quite low for lower power levels and rises sharply as power to the load is increased resulting in a nearly flat internal power dissipation over the normal operating range. Note that the internal dissipation at full output power is less than in the half power range. Calculating the efficiency for a specific system is the key to proper power supply design. For a 2.8-W audio system with 4-Ω loads and a 5-V supply, the maximum draw on the power supply is almost 3.8 W.

A final point to remember about Class-AB amplifiers is how to manipulate the terms in the efficiency equation to the utmost advantage when possible. Note that in Equation 3, VDD is in the denominator. This indicates that as VDD goes down, efficiency goes up.

Use Equation 4 as a simple formula for calculating the maximum power dissipated, PDmax, for a differential output application.

Equation 4. TPA6211A1 Q16_los367.gif

where

  • PDmax for a 5-V, 4-Ω system is 1.27 W.

The maximum ambient temperature depends on the heat sinking ability of the PCB system. The derating factor for the 3 mm ×3 mm DRB package is shown in the dissipation rating table. Converting this to θJA:

Equation 5. TPA6211A1 Q17_los367.gif

Given θJA, the maximum allowable junction temperature, and the maximum internal dissipation, the maximum ambient temperature can be calculated with Equation 6. The maximum recommended junction temperature for the TPA6211A1 is 150°C.

Equation 6. TPA6211A1 Q18_los367.gif

Equation 6 shows that the maximum ambient temperature is 91.7°C (package limited to 85°C ambient) at maximum power dissipation with a 5-V supply.

Table 2 shows that for most applications no airflow is required to keep junction temperatures in the specified range. The TPA6211A1 is designed with thermal protection that turns the device off when the junction temperature surpasses 150°C to prevent damage to the IC. In addition, using speakers with an impedance higher than 4-Ω dramatically increases the thermal performance by reducing the output current.

9.3.1.1 Advantages of Fully Differential Amplifiers

  • Input coupling capacitors not required: A fully differential amplifier with good CMRR, like the TPA6211A1, allows the inputs to be biased at voltage other than mid-supply. For example, if a DAC has a lower mid-supply voltage than that of the TPA6211A1, the common-mode feedback circuit compensates, and the outputs are still biased at the mid-supply point of the TPA6211A1. The inputs of the TPA6211A1 can be biased from 0.5 V to VDD - 0.8 V. If the inputs are biased outside of that range, input coupling capacitors are required.
  • Mid-supply bypass capacitor, C(BYPASS), not required: The fully differential amplifier does not require a bypass capacitor. Any shift in the mid-supply voltage affects both positive and negative channels equally, thus canceling at the differential output. Removing the bypass capacitor slightly worsens power supply rejection ratio (kSVR), but a slight decrease of kSVR may be acceptable when an additional component can be eliminated (See Figure 17).
  • Better RF-immunity: GSM handsets save power by turning on and shutting off the RF transmitter at a rate of 217 Hz. The transmitted signal is picked-up on input and output traces. The fully differential amplifier cancels the signal much better than the typical audio amplifier.
  • Figure 31 through Figure 38 show application schematics for differential and single-ended inputs.

9.3.1.2 Differential Output Versus Single-Ended Output

Figure 29 shows a Class-AB audio power amplifier (APA) in a fully differential configuration. The TPA6211A1 amplifier has differential outputs driving both ends of the load. One of several potential benefits to this configuration is power to the load. The differential drive to the speaker means that as one side is slewing up, the other side is slewing down, and vice versa. This in effect doubles the voltage swing on the load as compared to a ground-referenced load. Plugging 2 × VO(PP) into the power equation, where voltage is squared, yields 4× the output power from the same supply rail and load impedance Equation 7.

Equation 7. TPA6211A1 Q12_los367.gif
TPA6211A1 ai_diffout_los367.gif Figure 29. Differential Output Configuration

In a typical wireless handset operating at 3.6 V, bridging raises the power into an 8-Ω speaker from a singled-ended (SE, ground reference) limit of 200 mW to 800 mW. This is a 6-dB improvement in sound power—loudness that can be heard. In addition to increased power, there are frequency-response concerns. Consider the single-supply SE configuration shown in Figure 30. A coupling capacitor (CC) is required to block the dc-offset voltage from the load. This capacitor can be quite large (approximately 33 μF to 1000 μF) so it tends to be expensive, heavy, occupy valuable PCB area, and have the additional drawback of limiting low-frequency performance. This frequency-limiting effect is due to the high-pass filter network created with the speaker impedance and the coupling capacitance. This is calculated with Equation 8.

Equation 8. TPA6211A1 Q13_los367.gif

For example, a 68-μF capacitor with an 8-Ω speaker would attenuate low frequencies below 293 Hz. The BTL configuration cancels the dc offsets, which eliminates the need for the blocking capacitors. Low-frequency performance is then limited only by the input network and speaker response. Cost and PCB space are also minimized by eliminating the bulky coupling capacitor.

TPA6211A1 ai_dBfc_los367.gif Figure 30. Single-Ended Output and Frequency Response

Increasing power to the load does carry a penalty of increased internal power dissipation. The increased dissipation is understandable considering that the BTL configuration produces 4× the output power of the SE configuration.

9.4 Device Functional Modes

9.4.1 Shutdown Mode

The TPA6211A1 device can be put in shutdown mode when asserting SHUTDOWN pin to a logic LOW. While in shutdown mode, the device output stage is turned off and set into high impedance, making the current consumption very low. The device exits shutdown mode when a HIGH logic level is applied to SHUTDOWN pin.