ZHCSDC5B April 2014 – November 2019 TCA9546A
PRODUCTION DATA.
Following the successful acknowledgment of the slave address, the bus master sends a byte to the TCA9546A, which is stored in the control register (see Figure 14). If multiple bytes are received by the TCA9546A, it will save the last byte received. This register can be written and read via the I2C bus.