ZHCS275D July 2010 – January 2023 TCA6424A
PRODUCTION DATA
The Input Port registers (registers 0, 1 and 2) reflect the incoming logic levels of the pins, regardless of whether the pin is defined as an input or an output by the Configuration register. They act only on read operation. Writes to these registers have no effect. The default value (X) is determined by the externally applied logic level. Before a read operation, a write transmission is sent with the command byte to indicate to the I2C device that the Input Port register will be accessed next.
BIT | I-07 | I-06 | I-05 | I-04 | I-03 | I-02 | I-01 | I-00 |
DEFAULT | X | X | X | X | X | X | X | X |
BIT | I-17 | I-16 | I-15 | I-14 | I-13 | I-12 | I-11 | I-10 |
DEFAULT | X | X | X | X | X | X | X | X |
BIT | I-27 | I-26 | I-25 | I-24 | I-23 | I-22 | I-21 | I-20 |
DEFAULT | X | X | X | X | X | X | X | X |
The Output Port registers (registers 4, 5 and 6) shows the outgoing logic levels of the pins defined as outputs by the Configuration register. Bit values in these registers have no effect on pins defined as inputs. In turn, reads from these registers reflect the value that is in the flip-flop controlling the output selection, NOT the actual pin value.
BIT | O-07 | O-06 | O-05 | O-04 | O-03 | O-02 | O-01 | O-00 |
DEFAULT | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
BIT | O-17 | O-16 | O-15 | O-14 | O-13 | O-12 | O-11 | O-10 |
DEFAULT | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
BIT | O-27 | O-26 | O-25 | O-24 | O-23 | O-22 | O-21 | O-20 |
DEFAULT | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
The Polarity Inversion registers (registers 8, 9 and 10) allow polarity inversion of pins defined as inputs by the Configuration register. If a bit in these registers is set (written with 1), the corresponding port pin's polarity is inverted. If a bit in these registers is cleared (written with a 0), the corresponding port pin's original polarity is retained.
BIT | P-07 | P-06 | P-05 | P-04 | P-03 | P-02 | P-01 | P-00 |
DEFAULT | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
BIT | P-17 | P-16 | P-15 | P-14 | P-13 | P-12 | P-11 | P-10 |
DEFAULT | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
BIT | P-27 | P-26 | P-25 | P-24 | P-23 | P-22 | P-21 | P-20 |
DEFAULT | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
The Configuration registers (registers 12, 13 and 14) configure the direction of the I/O pins. If a bit in these registers is set to 1, the corresponding port pin is enabled as an input with a high-impedance output driver. If a bit in these registers is cleared to 0, the corresponding port pin is enabled as an output.
BIT | C-07 | C-06 | C-05 | C-04 | C-03 | C-02 | C-01 | C-00 |
DEFAULT | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
BIT | C-17 | C-16 | C-15 | C-14 | C-13 | C-12 | C-11 | C-10 |
DEFAULT | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
BIT | C-27 | C-26 | C-25 | C-24 | C-23 | C-22 | C-21 | C-20 |
DEFAULT | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |