ZHCSF35A October 2014 – June 2016 PGA300
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
The PGA 300 can be used in a variety of applications to measure pressure and temperature. Depending on the application, the device can be configured in different modes as illustrated in the following sections.
There are only a few requirements to take into account when using the PGA300 device in a design:
The EEPROM in the PGA300 is configured by default to operate in current mode using the OP_STG_CTRL register. If not, the following sequence must be followed to change it to current mode:
Voltage measured between the GND pin in the PGA300 device and the negative terminal of the controller. This includes the internal 40-Ω resistor and an external 10-Ω resistor, VPWR = 15 V. The DAC codes used were 0x880 and 0x2760 for 4 mA and 20 mA, respectively. |
There are only a few requirements to take into account when using the PGA300 in a design:
The following bits must be configured to reset the M0 microprocessor and to enable digital interface:
The following bits must be configured to turn ON the accurate reference buffer:
By turning on the accurate reference buffer, the reference voltage can be measured on REFCAP pin. Further, the capacitor on the REFCAP pin is connected to the reference buffer.
The following bits must be configured to turn on DAC and DAC GAIN:
There are only a few requirements to take into account when using the PGA300 in a design:
The following bits must be configured to reset the M0 microprocessor and to enable digital interface:
The following bits must be configured to turn ON the accurate reference buffer:
By turning on the accurate reference buffer, the reference voltage can be measured on REFCAP pin. Further, the capacitor on the REFCAP pin is connected to the reference buffer.
The following bits must be configured to turn on DAC and DAC GAIN: