ZHCSEI5A March 2013 – January 2016 LMX2485Q-Q1
PRODUCTION DATA.
请参考 PDF 数据表获取器件具体的封装图。
The LMX2485Q-Q1 consists of integrated N counters, R counters, and charge pumps. The TCXO, VCO and loop filter are supplied external to the chip.
The oscillator buffer must be driven single-ended by a signal source, such as a TCXO. The OSCout pin is included to provide a buffered output of this input signal and is active when the OSC_OUT bit is set to one. The ENOSC pin can be also pulled high to ensure that the OSCout pin is active, regardless of the status of the registers in the LMX2485Q-Q1.
The R counter divides this TXCO frequency down to the comparison frequency.
The maximum phase detector operating frequency for the IF PLL is straightforward, but it is a little more involved for the RF PLL because it is fractional. The maximum phase detector frequency for the LMX2485Q-Q1 RF PLL is 50 MHz. However, this is not possible in all circumstances due to illegal divide ratios of the N counter. The crystal reference frequency also limits the phase detector frequency, although the doubler helps with this limitation. There are trade-offs in choosing the phase detector frequency. If this frequency is run higher, then phase noise will be lower, but lock time may be increased due to cycle slipping and the capacitors in the loop filter may become rather large.
For the majority of the time, the charge pump output is high impedance, and the only current through this pin is the TRI-STATE leakage. However, it does put out fast correction pulses that have a width that is proportional to the phase error presented at the phase detector.
The charge pump converts the phase error presented at the phase detector into a correction current. The magnitude of this current is theoretically constant, but the duty cycle is proportional to the phase error. For the IF PLL, this current is not programmable, but for the RF PLL it is programmable in 16 steps. Also, the RF PLL allows for a higher charge pump current to be used when the PLL is locking in order to reduce the lock time.
The loop filter design can be rather involved. In addition to the regular constraints and design parameters, delta-sigma PLLs have the additional constraint that the order of the loop filter should be one greater than the order of the delta sigma modulator. This rule of thumb comes from the requirement that the loop filter must roll off the delta sigma noise at 20 dB/decade faster than it rises. However, because the noise can not have infinite power, it must eventually roll off. If the loop bandwidth is narrow, this requirement may not be necessary. For the purposes of discussion in this datasheet, the pole of the loop filter at 0 Hz is not counted. So a second order filter has 3 components, a 3rd order loop filter has 5 components, and the 4th order loop filter has 7 components. Although a 5th order loop filter is theoretically necessary for use with a 4th order modulator, typically a 4th order filter is used in this case. The loop filter design, especially for higher orders can be rather involved, but there are many simulation tools and references available, such as the one given at the end of the functional description block.
The N counter divides the VCO frequency down to the comparison frequency. Because prescalers are used, there are limitations on how small the N value can be. The N counters are discussed in greater depth in the Programming section. Because the input pins to these counters (FinRF and FinIF) are high frequency, layout considerations are important.
It is generally recommended that the VCO output go through a resistive pad and then through a DC-blocking capacitor before it gets to these high frequency input pins. If the trace length is sufficiently short (< 1/10th of a wavelength), then the pad may not be necessary, but a series resistor of about 39 Ω is still recommended to isolate the PLL from the VCO. The DC-blocking capacitor should be chosen at least to be 27 pF, depending on frequency. It may turn out that the frequency is above the self-resonant frequency of the capacitor, but because the input impedance of the PLL tends to be capacitive, it actually is a benefit to exceed the tune frequency. The pad and the DC-blocking capacitor should be placed as close to the PLL as possible
These inputs may be used to drive the PLL differentially, but it is very common to drive the PLL in a single ended fashion. A shunt capacitor should be placed at the FinRF* pin. The value of this capacitor should be chosen such that the impedance, including the ESR of the capacitor, is as close to an AC short as possible at the operating frequency of the PLL. 100 pF is a typical value, depending on frequency.
The RF PLL digital lock detect circuitry compares the difference between the phase of the inputs of the phase detector to a RC generated delay of ε. To indicate a locked state (Lock = HIGH) the phase error must be less than the ε RC delay for 5 consecutive reference cycles. Once in lock (Lock = HIGH), the RC delay is changed to approximately δ. To indicate an out of lock state (Lock = LOW), the phase error must become greater δ. The values of ε and δ are dependent on which PLL is used and are shown in Table 6:
PLL | ε | δ |
---|---|---|
RF | 10 ns | 20 ns |
IF | 15 ns | 30 ns |
When the PLL is in the power-down mode and the Ftest/LD pin is programmed for the lock detect function, it is forced LOW. The accuracy of this circuit degrades at higher comparison frequencies. To compensate for this, the DIV4 word should be set to one if the comparison frequency exceeds 20 MHz. The function of this word is to divide the comparison frequency presented to the lock detect circuit by 4.
NOTE
If the MUX[3:0] word is set such as to view lock detect for both PLLs, an unlocked (LOW) condition is shown whenever either one of the PLLs is determined to be out of lock.
The LMX2485Q-Q1 offers both cycle slip reduction (CSR) and Fastlock with timeout counter support. This means that it requires no additional programming overhead to use them. It is generally recommended that the charge pump current in the steady-state be 8X or less in order to use cycle slip reduction, and 4X or less in steady-state in order to use Fastlock. The next step is to decide between using Fastlock or CSR. This determination can be made based on the ratio of the comparison frequency (fCOMP) to loop bandwidth (BW).
COMPARISON FREQUENCY (fCOMP) |
FASTLOCK | CYCLE SLIP REDUCTION (CSR) |
---|---|---|
fCOMP ≤ 1.25 MHz | Noticeable better than CSR | Likely to provide a benefit, provided that fCOMP > 100 X BW |
1.25 MHz < fCOMP ≤ 2 MHz | Marginally better than CSR | |
fCOMP > 2 MHz | Same or worse than CSR |
Cycle slip reduction works by reducing the comparison frequency during frequency acquisition while keeping the same loop bandwidth, thereby reducing the ratio of the comparison frequency to the loop bandwidth. In cases where the ratio of the comparison frequency exceeds about 100 times the loop bandwidth, cycle slipping can occur and significantly degrade lock times. The greater this ratio, the greater the benefit of CSR. This is typically the case of high comparison frequencies. In circumstances where there is not a problem with cycle slipping, CSR provides no benefit. There is a glitch when CSR is disengaged, but because CSR should be disengaged long before the PLL is actually in lock, this glitch is not an issue. A good rule of thumb for CSR disengagement is to do this at the peak time of the transient response. Because this time is typically much sooner than Fastlock should be disengaged, it does not make sense to use CSR and Fastlock in combination.
Fastlock works by increasing the loop bandwidth only during frequency acquisition. In circumstances where the comparison frequency is less than or equal to 2 MHz, Fastlock may provide a benefit beyond what CSR can offer. Because Fastlock also reduces the ratio of the comparison frequency to the loop bandwidth, it may provide a significant benefit in cases where the comparison frequency is above 2 MHz. However, CSR can usually provide an equal or larger benefit in these cases, and can be implemented without using an additional resistor. The reason for this restriction on frequency is that Fastlock has a glitch when it is disengaged. As the time of engagement for Fastlock decreases and becomes on the order of the fast lock time, this glitch grows and limits the benefits of Fastlock. This effect becomes worse at higher comparison frequencies. There is always the option of reducing the comparison frequency at the expense of phase noise in order to satisfy this constraint on comparison frequency. Despite this glitch, there is still a net improvement in lock time using Fastlock in these circumstances. When using Fastlock, it is also recommended that the steady-state charge pump state be 4X or less. Also, Fastlock was originally intended only for second order filters, so when implementing it with higher order filters, the third and fourth poles can not be too close in, or it will not be possible to keep the loop filter well optimized when the higher charge pump current and Fastlock resistor are engaged.
Once it is decided that CSR is to be used, the cycle slip reduction factor needs to be chosen. The available factors are 1/2, 1/4, and 1/16. In order to preserve the same loop characteristics, TI recommends that Equation 4 be satisfied:
In order to satisfy this constraint, the maximum charge pump current in steady-state is 8X for a CSR of 1/2, 4X for a CSR of 1/4, and 1X for a CSR of 1/16. Because the PLL phase noise is better for higher charge pump currents, it makes sense to choose CSR only as large as necessary to prevent cycle slipping. Choosing it larger than this will not improve lock time, and will result in worse phase noise.
Consider an example where the desired loop bandwidth in steady-state is 100 kHz and the comparison frequency is 20 MHz. This yields a ratio of 200. Cycle slipping may be present, but would not be too severe if it was there. If a CSR factor of 1/2 is used, this would reduce the ratio to 100 during frequency acquisition, which is probably sufficient. A charge pump current of 8X could be used in steady-state, and a factor of 16X could be used during frequency acquisition. This yields a ratio of 1/2, which is equal to the CSR factor and this satisfies the above constraint. In this circumstance, it could also be decided to just use 16X charge pump current all the time, because it would probably have better phase noise, and the degradation in lock time would not be too severe.
Once it is decided that Fastlock is to be used, the loop bandwidth multiplier, K, is needed in order to determine the theoretical impact of Fastlock on the loop bandwidth and the resistor value, R2p, that is switched in parallel during Fastlock. This ratio is calculated in Equation 5:
K | LOOP BANDWIDTH | R2P VALUE | LOCK TIME |
---|---|---|---|
1 | 1.00 X | Open | 100 % |
2 | 1.41 X | R2/0.41 | 71 % |
3 | 1.73 X | R2/0.73 | 58% |
4 | 2.00 X | R2 | 50% |
8 | 2.83 X | R2/1.83 | 35% |
9 | 3.00 X | R2/2 | 33% |
16 | 4.00 X | R2/3 | 25% |
The above table shows how to calculate the Fastlock resistor and theoretical lock time improvement, once the ratio , K, is known. This all assumes a second order filter (not counting the pole at 0 Hz). However, it is generally recommended that the loop filter order be one greater than the order of the delta sigma modulator, which means that a second order filter is never recommended. In this case, the value for R2p is typically about 80% of what it would be for a second order filter. Because the Fastlock disengagement glitch gets larger and it is harder to keep the loop filter optimized as the K value becomes larger, designing for the largest possible value for K usually, but not always yields the best improvement in lock time. To get a more accurate estimate requires more simulation tools, or trial and error.
The LMX2485Q-Q1 has a high fractional modulus and high charge pump gain for the lowest possible phase noise. One consideration is that the reduced N value and higher charge pump may cause the capacitors in the loop filter to become larger in value. For larger capacitor values, it is common to have a trade-off between capacitor dielectric quality and physical size. Using film capacitors or NPO/COG capacitors yields the best possible lock times, where as using X7R or Z5R capacitors can increase lock time by 0 – 500%. However, it is a general tendency that designs that use a higher compare frequency tend to be less sensitive to the effects of capacitor dielectrics. Although the use of lesser quality dielectric capacitors may be unavoidable in many circumstances, allowing a larger footprint for the loop filter capacitors, using a lower charge pump current, and reducing the fractional modulus are all ways to reduce capacitor values. Capacitor dielectrics have very little impact on phase noise and spurs.
Control of the fractional spurs is more of an art than an exact science. The first differentiation that needs to be made is between primary fractional and sub-fractional spurs. The primary fractional spurs are those that occur at increments of the channel spacing only. The sub-fractional spurs are those that occur at a smaller resolution than the channel spacing, usually one-half or one-fourth. There are trade-offs between fractional spurs, sub-fractional spurs, and phase noise. The rules of thumb presented in this section are just that. There will be exceptions. The bits that impact the fractional spurs are FM and DITH, and these bits should be set in this order.
The first step to do is choose FM, for the delta sigma modulator order. TI recommends to start with FM = 3 for a third order modulator and use strong dithering. In general, there is a trade-off between primary and sub-fractional spurs. Choosing the highest order modulator (FM = 0 for 4th order) typically provides the best primary fractional spurs, but the worst sub-fractional spurs. Choosing the lowest modulator order (FM = 2 for 2nd order), typically gives the worst primary fractional spurs, but the best sub-fractional spurs. Choosing FM = 3, for a 3rd order modulator is a compromise.
The second step is to choose DITH, for dithering. Dithering has a very small impact on primary fractional spurs, but a much larger impact on sub-fractional spurs. The only problem is that it can add a few dB of phase noise, or even more if the loop bandwidth is very wide. Disabling dithering (DITH = 0), provides the best phase noise, but the sub-fractional spurs are worst (except when the fractional numerator is 0, and in this case, they are the best). Choosing strong dithering (DITH = 2) significantly reduces sub-fractional spurs, if not eliminating them completely, but adds the most phase noise. Weak dithering (DITH = 1) is a compromise.
The third step is to tinker with the fractional word. Although 1/10 and 400/4000 are mathematically the same, expressing fractions with much larger fractional numerators often improve the fractional spurs. Increasing the fractional denominator only improves spurs to a point. A good practical limit could be to keep the fractional denominator as large as possible, but not to exceed 4095, so it is not necessary to use the extended fractional numerator or denominator.
This steps can be done in different orders and it might take a few iterations to find the optimum performance. Special considerations should be taken for lower frequencies that are below about 100 MHz. In addition squaring up the wave, it is often helpful to use lowest terms fractions instead of highest terms fractions. Also, dithering may turn out to not be so useful. All the things are to introduce a methodical way of thinking about optimizing spurs, not an exact method. There will be exceptions to all these rules.
NOTE
For more information concerning delta-sigma PLLs, loop filter design, cycle slip reduction, Fastlock, and many other topics, visit ti.com/wireless. Here there is the EasyPLL simulation tool and an online reference called PLL Performance, Simulation, and Design.
TI recommends that all of the power pins be filtered with a series 18-Ω resistor and then placing two capacitors shunt to ground, thus creating a low pass filter. Although it makes sense to use large capacitor values in theory, the ESR (Equivalent Series Resistance) is greater for larger capacitors. For optimal filtering minimize the sum of the ESR and theoretical impedance of the capacitor. It is therefore recommended to provide two capacitors of very different sizes for the best filtering. 1 µF and 100 pF are typical values. The small capacitor should be placed as close as possible to the pin.
The power down state of the LMX2485Q-Q1 is controlled by many factors. The one factor that overrides all other factors is the CE pin. If this pin is low, the part will be powered down. Asserting a high logic level on this pin is necessary to power up the chip, however, there are other bits in the programming registers that can override this and put the PLL back in a power down state. Provided that the voltage on the CE pin is high, programming the RF_PD and IF_PD bits to zero specifies that the part will be powered up. Programming either one of these bits to one will power down the appropriate section of the synthesizer, provided that the ATPU bit does not override this.
CE Pin | RF_PD | ATPU BIT ENABLED + N Counter Write |
PLL STATE |
---|---|---|---|
Low | X | X | Powered Down (Asynchronous) |
High | X | Yes | Powered Up |
High | 0 | No | Powered Up |
High | 1 | No | Powered Down (Asynchronous) |
The 24-bit data registers are loaded through a MICROWIRE Interface. These data registers are used to program the R counter, the N counter, and the internal mode control latches. The data format of a typical 24-bit data register is shown below. The control bits CTL [3:0] decode the register address. On the rising edge of LE, data stored in the shift register is loaded into one of the appropriate latches (selected by address bits). Data is shifted in MSB first.
NOTE
It is best to program the N counter last, because doing so initializes the digital lock detector and Fastlock circuitry. Note that initialize means it resets the counters, but it does NOT program values into these registers. The exception is when 22-bit is not being used. In this case, it is not necessary to program the R7 register.
MSB | LSB | ||||
---|---|---|---|---|---|
DATA [21:0] | CTL [3:0] | ||||
23 | 4 | 3 | 2 | 1 | 0 |
The control bits CTL [3:0] decode the internal register address. The table below shows how the control bits are mapped to the target control register.
C3 | C2 | C1 | C0 | DATA Location |
---|---|---|---|---|
x | x | x | 0 | R0 |
0 | 0 | 1 | 1 | R1 |
0 | 1 | 0 | 1 | R2 |
0 | 1 | 1 | 1 | R3 |
1 | 0 | 0 | 1 | R4 |
1 | 0 | 1 | 1 | R5 |
1 | 1 | 0 | 1 | R6 |
1 | 1 | 1 | 1 | R7 |
Because the LMX2485Q-Q1 registers are complicated, they are organized into two groups, basic and advanced. The first four registers are basic registers that contain critical information necessary for the PLL to achieve lock. The last 5 registers are for features that optimize spur, phase noise, and lock time performance. The next page shows these registers.
Although it is highly recommended that the user eventually take advantage of all the modes of the LMX2485, the quick start register map is shown in order for the user to get the part up and running quickly using only those bits critical for basic functionality. The following default conditions for this programming state are a third order delta-sigma modulator in 12-bit mode with no dithering and no Fastlock.
REGISTER | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 | |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
DATA[19:0] (Except for the RF_N Register, which is [22:0]) | C3 | C2 | C1 | C0 | |||||||||||||||||||||
R0 | RF_N[10:0] | RF_FN[11:0] | 0 | ||||||||||||||||||||||
R1 | RF_ PD |
RF_P | RF_R[5:0] | RF_FD[11:0] | 0 | 0 | 1 | 1 | |||||||||||||||||
R2 | IF_PD | IF_N[18:0] | 0 | 1 | 0 | 1 | |||||||||||||||||||
R3 | 0001 | RF_CPG[3:0] | IF_R[11:0] | 0 | 1 | 1 | 1 | ||||||||||||||||||
R4 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 0 | 0 | 1 | 1 | 1 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 |
The complete register map shows all the functionality of all registers, including the last five.
REGISTER | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
DATA[19:0] (Except for the RF_N Register, which is [22:0]) | C3 | C2 | C1 | C0 | ||||||||||||||||||||
R0 | RF_N[10:0] | RF_FN[11:0] | 0 | |||||||||||||||||||||
R1 | RF_ PD |
RF_P | RF_R[5:0] | RF_FD[11:0] | 0 | 0 | 1 | 1 | ||||||||||||||||
R2 | IF_ PD |
IF_N[18:0] | 0 | 1 | 0 | 1 | ||||||||||||||||||
R3 | ACCESS[3:0] | RF_CPG[3:0] | IF_R[11:0] | 0 | 1 | 1 | 1 | |||||||||||||||||
R4 | ATPU | 0 | 1 | 0 | 0 | 0 | DITH [1:0] |
FM [1:0] |
0 | OSC _2X |
OSC _OUT |
IF_ CPP |
RF_ CPP |
IF_P | MUX [3:0] |
1 | 0 | 0 | 1 | |||||
R5 | RF_FD[21:12] | RF_FN[21:12] | 1 | 0 | 1 | 1 | ||||||||||||||||||
R6 | CSR[1:0] | RF_CPF[3:0] | RF_TOC[13:0] | 1 | 1 | 0 | 1 | |||||||||||||||||
R7 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | DIV4 | 0 | 1 | 0 | 0 | 1 | IF_ RST |
RF_ RST |
IF_ CPT |
RF_ CPT |
1 | 1 | 1 | 1 |
NOTE
This register has only one control bit, so the N counter value to be changed with a single write statement to the PLL.
23 | 13 | 12 | 1 | 0 | |||||||||||||||||||
RF_N[10:0] | RF_FN[11:0] | 0 |
BIT | FIELD | DESCRIPTION |
---|---|---|
23-13 | RF_N[10:0] |
RF N Counter Value The RF N counter contains an 8/9/12/13 and a 16/17/20/21 prescaler. The N counter value can be calculated as follows: N = RF_P·RF_C + 4·RF_B + RF_A RF_C ≥Max{RF_A, RF_B} , for N-2FM-1 ... N+2FM is a necessary condition. This rule is slightly modified in the case where the RF_B counter has an unused bit, where this extra bit is used by the delta-sigma modulator for the purposes of modulation. Consult the tables below for valid operating ranges for each prescaler. |
12-1 | RF_FN[11:0] |
Fractional Numerator for RF PLL Refer to Table 33 for a more detailed description of this control word. |
RF_N | RF_N [10:0] | ||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|
RF_C [6:0] | RF_B [1:0] | RF_A [1:0] | |||||||||
<25 | N values less than 25 are prohibited. | ||||||||||
25-26 | Possible only with a second order delta-sigma engine. | ||||||||||
27-30 | Possible only with a second or third order delta-sigma engine. | ||||||||||
31 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 1 | 1 | 1 |
... | . | . | . | . | . | . | . | 0 | . | . | . |
1023 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0 | 1 | 1 | 1 |
>1023 | N values above 1023 are prohibited. |
RF_N | RF_N [10:0] | ||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|
RF_C [6:0] | RF_B [1:0] | RF_A [1:0] | |||||||||
<49 | N values less than 49 are prohibited. | ||||||||||
49-50 | Possible only with a second order delta-sigma engine. | ||||||||||
51-54 | Possible with a second or third order delta-sigma engine. | ||||||||||
55 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 1 | 1 | 1 |
... | . | . | . | . | . | . | . | . | . | . | . |
2039 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0 | 1 | 1 | 1 |
2040-2043 | Possible with a second or third order delta-sigma engine. | ||||||||||
2044-2045 | Possible only with a second order delta-sigma engine. | ||||||||||
>2045 | N values greater than 2045 are prohibited. |
23 | 22 | 21 | 16 | 15 | 4 | 3 | 2 | 1 | 0 | ||||||||||||||
RF_PD | RF_P | RF_R[5:0] | RF_FD[11:0] | 0 | 0 | 1 | 1 |
BIT | FIELD | DESCRIPTION |
---|---|---|
23 | RF_PD |
RF Power Down Control Bit When this bit is set to 0, the RF PLL operates normally. When it is set to one, the RF PLL is powered down and the RF Charge pump is set to a TRI-STATE mode. The CE pin and ATPU bit also control power down functions, and will override the RF_PD bit. The order of precedence is as follows. First, if the CE pin is LOW, then the PLL will be powered down. Provided this is not the case, the PLL will be powered up if the ATPU bit says to do so, regardless of the state of the RF_PD bit. After the CE pin and the ATPU bit are considered, then the RF_PD bit then takes control of the power down function for the RF PLL. |
22 | RF_P |
RF Prescaler bit The prescaler used is determined by this bit. |
21-16 | RF_R[5:0] |
RF R Divider Value The RF R Counter value is determined by this control word. Note that this counter does allow values down to one. The RF R Counter value is determined by this control word. Note that this counter does allow values down to one. |
15-4 | RF_FD[11:0] |
RF PLL Fractional Denominator The function of these bits are described in Table 34. |
R Value | RF_R[5:0] | |||||
---|---|---|---|---|---|---|
1 | 0 | 0 | 0 | 0 | 0 | 1 |
... | . | . | . | . | . | . |
63 | 1 | 1 | 1 | 1 | 1 | 1 |
RF_P | PRESCALER | MAXIMUM FREQUENCY |
---|---|---|
0 | 8/9/12/13 | 2000 MHz |
1 | 16/17/20/21 | 3000 MHz |
23 | 22 | 4 | 3 | 2 | 1 | 0 | |||||||||||||||||
IF_PD | IF_N[18:0] | 0 | 1 | 0 | 1 |
BIT | FIELD | DESCRIPTION |
---|---|---|
23 | IF_PD |
IF Power Down Bit When this bit is set to 0, the IF PLL operates normally. When it is set to 1, the IF PLL powers down and the output of the IF PLL charge pump is set to a TRI-STATE mode. If the ATPU bit is set and register R0 is written to, the IF_PD will be reset to 0 and the IF PLL will be powered up. If the CE pin is held low, the IF PLL will be powered down, overriding the IF_PD bit. |
22-4 | IF_N[18:0] |
IF N Divider Value |
N VALUE | IF_N[18:0] | ||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
IF_B | IF_A | ||||||||||||||||||
≤23 | N values less than or equal to 23 are prohibited because IF_B ≥ 3 is required. | ||||||||||||||||||
24-55 | Legal divide ratios in this range are: 24-27, 32-36, 40-45, 48-54 |
||||||||||||||||||
56 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 0 | 0 | 0 | 0 |
57 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 0 | 0 | 0 | 1 |
... | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . |
262143 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 0 | 1 | 1 | 1 |
N VALUE | IF_B | IF_A | |||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
≤47 | N values less than or equal to 47 are prohibited because IF_B ≥ 3 is required. | ||||||||||||||||||
48-239 | Legal divide ratios in this range are: 48-51, 64-68, 80-85, 96-102, 112-119, 128-136, 144-153, 160-170, 176-187, 192-204, 208-221, 224-238 |
||||||||||||||||||
240 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 0 |
241 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 1 | 0 | 0 | 0 | 1 |
... | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . |
524287 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
23 | 20 | 19 | 16 | 15 | 4 | 3 | 2 | 1 | 0 | ||||||||||||||
ACCESS[3:0] | RF_CPG[3:0] | IF_R[11:0] | 0 | 1 | 1 | 0 |
BIT | FIELD | DESCRIPTION |
---|---|---|
23-20 | ACCESS[3:0] |
Register Access word It is mandatory that the first 5 registers R0-R4 be programmed. The programming of registers R5-R7 is optional. The ACCESS[3:0] bits determine which additional registers need to be programmed. Any one of these registers can be individually programmed. According to the table below, when the state of a register is in default mode, all the bits in that register are forced to a default state and it is not necessary to program this register. When the register is programmable, it needs to be programmed through the MICROWIRE. Using this register access technique, the programming required is reduced up to 37%. |
19-16 | RF_CPG[3:0] |
RF PLL Charge Pump Gain This is used to control the magnitude of the RF PLL charge pump in steady-state operation. |
15-4 | IF_R[11:0] |
IF R Divider Value For the IF R divider, the R value is determined by the IF_R[11:0] bits in the R3 register. The minimum value for IF_R is 3. |
R VALUE | IF_R[11:0] | |||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|
3 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 |
... | . | . | . | . | . | . | . | . | . | . | . | . |
4095 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
RF_CPG | CHARGE PUMP STATE | TYPICAL RF CHARGE PUMP CURRENT AT 3 VOLTS (µA) |
---|---|---|
0 | 1X | 95 |
1 | 2X | 190 |
2 | 3X | 285 |
3 | 4X | 380 |
4 | 5X | 475 |
5 | 6X | 570 |
6 | 7X | 665 |
7 | 8X | 760 |
8 | 9X | 855 |
9 | 10X | 950 |
10 | 11X | 1045 |
11 | 12X | 1140 |
12 | 13X | 1235 |
13 | 14X | 1330 |
14 | 15X | 1425 |
15 | 16X | 1520 |
ACCESS BIT | REGISTER LOCATION | REGISTER CONTROLLED |
---|---|---|
ACCESS[0] | R3[20] | Must be set to 1 |
ACCESS[1] | R3[21] | R5 |
ACCESS[2] | R3[22] | R6 |
ACCESS[3] | R3[23] | R7 |
The default conditions the registers is shown below:
REGISTER | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Data[19:0] | C3 | C2 | C1 | C0 | ||||||||||||||||||||
R4 | R4 Must be programmed manually. | |||||||||||||||||||||||
R5 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 1 | 1 |
R6 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 1 | 0 | 1 |
R7 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 1 | 1 | 1 | 1 |
This corresponds to the following bit settings.
REGISTER | BIT LOCATION | BIT NAME | BIT DESCRIPTION | BIT VALUE | BIT STATE |
---|---|---|---|---|---|
R4 | R4[23] | ATPU | Autopowerup | 0 | Disabled |
R4[17:16] | DITH | Dithering | 2 | Strong | |
R4[15:14] | FM | Modulation Order | 3 | 3rd Order | |
R4[12] | OSC_2X | Oscillator Doubler | 0 | Disabled | |
R4[11] | OSC_OUT | OSCout Pin Enable | 0 | Disabled | |
R4[10] | IF_CPP | IF Charge Pump Polarity | 1 | Positive | |
R4[9] | RF_CPP | RF Charge Pump Polarity | 1 | Positive | |
R4[8] | IF_P | IF PLL Prescaler | 1 | 16/17 | |
R4[7:4] | MUX | Ftest/LD Output | 0 | Disabled | |
R5 | R5[23:14] | RF_FD[21:12] | Extended Fractional Denominator | 0 | Disabled |
R5[13:4] | RF_FN[21:12] | Extended Fractional Numerator | 0 | Disabled | |
R6 | R6[23:22] | CSR | Cycle Slip Reduction | 0 | Disabled |
R6[21:18] | RF_CPF | Fastlock Charge Pump Current | 0 | Disabled | |
R6[17:4] | RF_TOC | RF Timeout Counter | 0 | Disabled | |
R7 | R7[13] | DIV4 | Lock Detect Adjustment | 0 | Disabled (Fcomp ≤ 20 MHz) |
R7[7] | IF_RST | IF PLL Counter Reset | 0 | Disabled | |
R7[6] | RF_RST | RF PLL Counter Reset | 0 | Disabled | |
R7[5] | IF_CPT | IF PLL Tri-State | 0 | Disabled | |
R7[4] | RF_CPT | RF PLL Tri-State | 0 | Disabled |
This register controls the conditions for the RF PLL in Fastlock.
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 |
ATPU | 0 | 1 | 0 | 0 | 0 | DITH[1:0] | FM[1:0] | 0 | OSC_2X | ||
11 | 10 | 9 | 8 | 7 | 4 | 3 | 2 | 1 | 0 | ||
OSC_OUT | IF_CPP | RF_CPP | IF_P | MUX[3:0] | 1 | 0 | 0 | 1 |
BIT | FIELD | DESCRIPTION |
---|---|---|
23 | ATPU |
PLL Automatic Power Up When this bit is set to 1, both the RF and IF PLL power up when the R0 register is written to. When the R0 register is written to, the PD_RF and PD_IF bits are changed to 0 in the PLL registers. The exception to this case is when the CE pin is low. In this case, the ATPU function is disabled. |
17-16 | DITH[1:0] |
Dithering Control Dithering is a technique used to spread out the spur energy. Enabling dithering can reduce the main fractional spurs, but can also give rise to a family of smaller spurs. Whether dithering helps or hurts is application specific. Enabling the dithering may also increase the phase noise. In most cases where the fractional numerator is zero, dithering usually degrades performance. Dithering tends to be most beneficial in applications where there is insufficient filtering of the spurs. This often occurs when the loop bandwidth is very wide or a higher order delta-sigma modulator is used. Dithering tends not to impact the main fractional spurs much, but has a much larger impact on the sub-fractional spurs. If it is decided that dithering will be used, best results will be obtained when the fractional denominator is at least 1000. 0 = Disabled 1 = Weak Dithering 2 = Strong Dithering 3 = Reserved |
15-14 | FM[1:0] |
Fractional Mode Determines the order of the delta-sigma modulator. Higher order delta-sigma modulators reduce the spur levels closer to the carrier by pushing this noise to higher frequency offsets from the carrier. In general, the order of the loop filter should be at least one greater than the order of the delta-sigma modulator in order to allow for sufficient roll-off. 0 = Fractional PLL mode with a 4th order delta-sigma modulator 1 = Disable the delta-sigma modulator. Recommended for test use only. 2 = Fractional PLL mode with a 2nd order delta-sigma modulator 3 = Fractional PLL mode with a 3rd order delta-sigma modulator |
12 | OSC_2X |
Oscillator Doubler Enable When this bit is set to 0, the oscillator doubler is disabled and the TCXO frequency presented to the IF R and RF R counters is equal to that of the input frequency of the OSCin pin. When this bit is set to 1, the TCXO frequency presented to the RF R counter is doubled. Phase noise added by the doubler is negligible. |
11 | OSC_OUT |
Oscillator Output Buffer Enable 0 = Disabled (High Impedance) 1 = Buffered output of OSCin pin |
10 | IF_CPP |
IF PLL Charge Pump Polarity For a positive phase detector polarity, which is normally the case, set this bit to 1. Otherwise set this bit for a negative phase detector polarity. 0 = Negative 1 = Positive |
9 | RF_CPP |
RF PLL Charge Pump Polarity 0 = Negative 1 = Positive (Default) |
8 | IF_P |
IF Prescaler When this bit is set to 0, the 8/9 prescaler is used. Otherwise the 16/17 prescaler is used. |
7-4 | MUX[3:0] |
Frequency Out & Lock Detect MUX These bits determine the output state of the Ftest/LD pin. |
MUX[3:0] | OUTPUT TYPE | OUTPUT DESCRIPTION | |||
---|---|---|---|---|---|
0 | 0 | 0 | 0 | High Impedance | Disabled |
0 | 0 | 0 | 1 | Push-Pull | General-purpose output, Logical “High” State |
0 | 0 | 1 | 0 | Push-Pull | General-purpose output, Logical “Low” State |
0 | 0 | 1 | 1 | Push-Pull | RF & IF Digital Lock Detect |
0 | 1 | 0 | 0 | Push-Pull | RF Digital Lock Detect |
0 | 1 | 0 | 1 | Push-Pull | IF Digital Lock Detect |
0 | 1 | 1 | 0 | Open Drain | RF & IF Analog Lock Detect |
0 | 1 | 1 | 1 | Open Drain | RF Analog Lock Detect |
1 | 0 | 0 | 0 | Open Drain | IF Analog Lock Detect |
1 | 0 | 0 | 1 | Push-Pull | RF & IF Analog Lock Detect |
1 | 0 | 1 | 0 | Push-Pull | RF Analog Lock Detect |
1 | 0 | 1 | 1 | Push-Pull | IF Analog Lock Detect |
1 | 1 | 0 | 0 | Push-Pull | IF R Divider divided by 2 |
1 | 1 | 0 | 1 | Push-Pull | IF N Divider divided by 2 |
1 | 1 | 1 | 0 | Push-Pull | RF R Divider divided by 2 |
1 | 1 | 1 | 1 | Push-Pull | RF N Divider divided by 2 |
IF_P | IF PRESCALER | MAXIMUM FREQUENCY |
---|---|---|
0 | 8/9 | 800 MHz |
1 | 16/17 | 800 MHz |
OSC2X | FREQUENCY PRESENTED TO RF R COUNTER | FREQUENCY PRESENTED TO IF R COUNTER |
---|---|---|
0 | fOSCin | fOSCin |
1 | 2 x fOSCin |
23 | 14 | 13 | 4 | 3 | 2 | 1 | 0 | ||||||||||||||||
RF_FD[21:12] | RF_FN[21:12] | 1 | 0 | 1 | 1 |
In the case that the ACCESS[1] bit is 0, then the part operates in 12-bit fractional mode, and the RF_FN2[21:12] bits become do not care bits. When the ACCESS[1] bit is set to 1, the part operates in 22-bit mode and the fractional numerator is expanded from 12 to 22-bits.
FRACTIONAL | RF_FN[21:12] | RF_FN[11:0] | ||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
NUMERATOR | (These bits only apply in 22-bit mode) | |||||||||||||||||||||
0 | In 12-bit mode, these are do not care. In 22-bit mode, for N <4096, these bits should be all set to 0. |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |||||||||
1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | ||||||||||
... | . | . | . | . | . | . | . | . | . | . | . | . | ||||||||||
4095 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | ||||||||||
4096 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
... | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . |
4194303 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
In the case that the ACCESS[1] bit is 0, then the part is operates in the 12-bit fractional mode, and the RF_FD[21:12] bits become do not care bits. When the ACCESS[1] is set to 1, the part operates in 22-bit mode and the fractional denominator is expanded from 12 to 22-bits.
FRACTIONAL | RF_FD[21:12] | RF_FD[11:0] | ||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
DENOMINATOR | (These bits only apply in 22-bit mode) | |||||||||||||||||||||
0 | In 12-bit mode, these are do not care. In 22-bit mode, for N <4096, these bits should be all set to 0. |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | |||||||||
1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | ||||||||||
... | . | . | . | . | . | . | . | . | . | . | . | . | ||||||||||
4095 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | ||||||||||
4096 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
... | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . | . |
4194303 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 | 1 |
23 | 22 | 21 | 18 | 17 | 4 | 3 | 2 | 1 | 0 | ||||||||||||||
CSR[1:0] | RF_CPF[3:0] | RF_TOC[13:0] | 1 | 1 | 0 | 1 |
BIT | FIELD | DESCRIPTION |
---|---|---|
23-22 | CSR[1:0] |
RF Cycle Slip Reduction CSR controls the operation of the Cycle Slip Reduction Circuit. This circuit can be used to reduce the occurrence of phase detector cycle slips. Note that the Fastlock charge pump current, steady-state current, and CSR control are all interrelated. Refer to Cycle Slip Reduction and Fastlock for information on how to use this. |
21-18 | RF_CPF[3:0] |
RF PLL Fastlock Charge Pump Current Specify the charge pump current for the Fastlock operation mode for the RF PLL. Note that the Fastlock charge pump current, steady-state current, and CSR control are all interrelated. |
17-4 | RF_TOC[13:0] |
RF Time Out Counter and Control for FLoutRF Pin The RF_TOC[13:0] word controls the operation of the RF Fastlock circuitry as well as the function of the FLoutRF output pin. When this word is set to a value between 0 and 3, the RF Fastlock circuitry is disabled and the FLoutRF pin operates as a general-purpose CMOS TRI-STATE I/O. When RF_TOC is set to a value between 4 and 16383, the RF Fastlock mode is enabled and the FLoutRF pin is utilized as the RF Fastlock output pin. The value programmed into the RF_TOC[13:0] word represents two times the number of phase detector comparison cycles the RF synthesizer will spend in the Fastlock state. |
RF_TOC | FASTLOCK MODE | Fastlock Period [CP events] | FLoutRF PIN FUNCTIONALITY |
---|---|---|---|
0 | Disabled | N/A | High Impedance |
1 | Manual | N/A | Logic 0 State. Forces all Fastlock conditions |
2 | Disabled | N/A | Logic 0 State |
3 | Disabled | N/A | Logic 1 State |
4 | Enabled | 4X2 = 8 | Fastlock |
5 | Enabled | 5X2 = 10 | Fastlock |
… | Enabled | … | Fastlock |
16383 | Enabled | 16383X2 = 32766 | Fastlock |
RF_CPF | RF CHARGE PUMP STATE | TYPICAL RF CHARGE PUMP CURRENT AT 3 VOLTS (µA) |
---|---|---|
0 | 1X | 95 |
1 | 2X | 190 |
2 | 3X | 285 |
3 | 4X | 380 |
4 | 5X | 475 |
5 | 6X | 570 |
6 | 7X | 665 |
7 | 8X | 760 |
8 | 9X | 855 |
9 | 10X | 950 |
10 | 11X | 1045 |
11 | 12X | 1140 |
12 | 13X | 1235 |
13 | 14X | 1330 |
14 | 15X | 1425 |
15 | 16X | 1520 |
CSR | CSR STATE | SAMPLE RATE REDUCTION FACTOR |
---|---|---|
0 | Disabled | 1 |
1 | Enabled | 1/2 |
2 | Enabled | 1/4 |
3 | Enabled | 1/16 |
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
0 | 0 | DIV4 | 0 | 1 | 0 | 0 | 1 |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
IF_RST | RF_RST | IF_CPT | RF_CPT | 1 | 1 | 1 | 1 |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
BIT | FIELD | DESCRIPTION |
---|---|---|
13 | DIV4 |
RF Digital Lock Detect Divide By 4 Because the digital lock detect function is based on a phase error, it becomes more difficult to detect a locked condition for larger comparison frequencies. When this bit is enabled, it subdivides the RF PLL comparison frequency (it does not apply to the IF comparison frequency) presented to the digital lock detect circuitry by 4. This enables this circuitry to work at higher comparison frequencies. TI recommends that this bit be enabled whenever the comparison frequency exceeds 20 MHz and RF digital lock detect is being used. |
7 | IF_RST |
IF PLL Counter Reset When this bit is enabled, the IF PLL N and R counters are reset, and the charge pump is put in a Tri-State condition. This feature should be disabled for normal operation. Note that a counter reset is applied whenever the chip is powered up through software or CE pin. |
6 | RF_RST |
RF PLL Counter Reset When this bit is enabled, the RF PLL N and R counters are reset and the charge pump is put in a Tri-State condition. This feature should be disabled for normal operation. This feature should be disabled for normal operation. Note that a counter reset is applied whenever the chip is powered up through software or CE pin. |
5 | IF_CPT |
IF Charge Pump Tri-State When this bit is enabled, the IF PLL charge pump is put in a Tri-State condition, but the counters are not reset. This feature is typically disabled for normal operation. |
4 | RF_CPT |
RF Charge Pump Tri-State When this bit is enabled, the RF PLL charge pump is put in a Tri-State condition, but the counters are not reset. This feature is typically disabled for normal operation. |
IF_RST | IF PLL N AND R COUNTERS | IF PLL CHARGE PUMP |
---|---|---|
0 (Default) | Normal Operation | Normal Operation |
1 | Counter Reset | Tri-State |
RF_RST | RF PLL N AND R COUNTERS | RF PLL CHARGE PUMP |
---|---|---|
0 (Default) | Normal Operation | Normal Operation |
1 | Counter Reset | Tri-State |
RF_TRI | RF PLL N AND R COUNTERS | RF PLL CHARGE PUMP |
---|---|---|
0 (Default) | Normal Operation | Normal Operation |
1 | Normal Operation | Tri-State |
IF_TRI | IF PLL N AND R COUNTERS | IF PLL CHARGE PUMP |
---|---|---|
0 (Default) | Normal Operation | Normal Operation |
1 | Normal Operation | Tri-State |