The VIN terminal is recommended to have a low-ESR ceramic bypass-capacitor. The typical recommended bypass capacitance is a 10-μF ceramic capacitor with a X5R or X7R dielectric.
The VIN terminal must be tied to the source of the MOSFET using a thick trace or polygon.
The Anode pin of the LM74670-Q1 is connected to the Source of the MOSFET for sensing.
The Cathode pin of the LM74670-Q1 is connected to the drain of the MOSFET for sensing.
The high current path of for this solution is through the MOSFET, therefor it is important to use thick traces for source and drain of the MOSFET.
The charge pump capacitor Vcap must be kept away from the MOSFET to lower the thermal effects on the capacitance value.
The Gate Drive and Gate pull down pins of the LM74670-Q1 must be connected to the MOSFET gate without using vias.
Obtaining acceptable performance with alternate layout schemes is possible, however this layout has been shown to produce good results and is intended as a guideline.