ZHCSTL8F April 2007 – November 2023 LM25116
PRODUCTION DATA
PIN | TYPE(1) | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | VIN | P | Chip supply voltage, input voltage monitor and input to the VCC regulator. |
2 | UVLO | I | If the UVLO pin is below 1.215 V, the regulator is in standby mode (VCC regulator running, switching regulator disabled). If the UVLO pin voltage is above 1.215 V, the regulator is operational. An external voltage divider can be used to set an undervoltage shutdown threshold. There is a fixed 5 µA pull up current on this pin when EN is high. UVLO is pulled to ground in the event a current limit condition exists for 256 clock cycles. |
3 | RT/SYNC | I | The internal oscillator is set with a single resistor between this pin and the AGND pin. The recommended frequency range is 50 kHz to 1 MHz. The internal oscillator can be synchronized to an external clock by AC coupling a positive edge onto this node. |
4 | EN | I | If the EN pin is below 0.5 V, the regulator is in a low power state drawing less than 10 µA from VIN. EN must be pulled above 3.3 V for normal operation. |
5 | RAMP | I | Ramp control signal. An external capacitor connected between this pin and the AGND pin sets the ramp slope used for current mode control. |
6 | AGND | G | Analog ground. Connect to PGND through the exposed pad ground connection under the LM25116. |
7 | SS | I | An external capacitor and an internal 10-µA current source set the soft start time constant for the rise of the error amp reference. The SS pin is held low during VCC < 4.5 V, UVLO < 1.215 V, EN input low or thermal shutdown. |
8 | FB | I | Feedback signal from the regulated output. This pin is connected to the inverting input of the internal error amplifier. The regulation threshold is 1.215 V. |
9 | COMP | O | Output of the internal error amplifier. The loop compensation network must be connected between this pin and the FB pin. |
10 | VOUT | I | Output monitor. Connect directly to the output voltage. |
11 | DEMB | I | Low-side MOSFET source voltage monitor for diode emulation. For start-up into a pre-biased load, tie this pin to ground at the CSG connection. For fully synchronous operation, use an external series resistor between DEMB and ground to raise the diode emulation threshold above the low-side SW on-voltage. |
12 | CS | I | Current sense amplifier input. Connect to the top of the current sense resistor or the drain of the low-sided MOSFET if RDS(ON) current sensing is used. |
13 | CSG | G | Current sense amplifier input. Connect to the bottom of the sense resistor or the source of the low-side MOSFET if RDS(ON) current sensing is used. |
14 | PGND | G | Power ground. Connect to AGND through the exposed pad ground connection under the LM25116. |
15 | LO | O | Connect to the gate of the low-side synchronous MOSFET through a short, low inductance path. |
16 | VCC | P | Locally decouple to PGND using a low ESR/ESL capacitor placed as close to the controller as possible. |
17 | VCCX | P | Optional input for an externally supplied VCC. If VCCX > 4.5 V, VCCX is internally connected to VCC and the internal VCC regulator is disabled. If VCCX is unused, it must be connected to ground. |
18 | HB | P | High-side driver supply for bootstrap gate drive. Connect to the cathode of the bootstrap diode and the positive terminal of the bootstrap capacitor. The bootstrap capacitor supplies current to charge the high-side MOSFET gate and must be placed as close to the controller as possible. |
19 | HO | O | Connect to the gate of the high-side synchronous MOSFET through a short, low inductance path |
20 | SW | O | Switch node. Connect to the negative terminal of the bootstrap capacitor and the source terminal of the high-side MOSFET. |
EP | EP | — | Exposed pad. Solder to ground plane. |