选择版本
SIMPLELINK-CC32XX-SDK
SimpleLink™ Wi-Fi® CC32xx 软件开发套件 (SDK)
Link to Windows Installer for SimpleLink CC32XX SDK
Link to macOS Installer for SimpleLink CC32XX SDK
Link to Linux Installer for SimpleLink CC32XX SDK
Link to Windows Installer for SimpleLink CC3x20 Service Pack
Link to Mac Installer for SimpleLink CC3x20 Service Pack
Link to Linux Installer for SimpleLink CC3x20 Service Pack
Link to Radio Tool for SimpleLink CC32XX SDK and SimpleLink SDK Wi-Fi Plug-In
产品
Wi-Fi 产品
硬件开发
文档
SimpleLink CC32XX SDK Documentation
发布信息
Click on the links in the table above to download. The SimpleLink Wi-Fi SDK delivers components that enable engineers to develop connected applications on Texas Instruments Wi-Fi micro-controller devices. The product is comprised of multiple software components and examples of how to use these components together. In addition, examples are provided to demonstrate the use of each functional area and each supported device and as a starting point for your own projects.
For CC3220 SDK versions 2.30 and earlier, please see the CC3220 SDK download page.
最新动态
SimpleLink SDK 3.10.00.04
- MDNS updates to support BCT 1.4 certification
- SimpleLink host driver - please refer to the Doxygen for full API information and usage
- Added API to retrieve the beacon interval and DTIM count when connected to an Access Point (sl_WlanGet)
- Added API to retrieve device time/power statistics from the MAC layer and the network processor (sl_DeviceGet)
- Various bug fixes
SimpleLink CC3x20 Service Pack 3.11.1.0-2.0.0.0-2.2.0.6 - Released June 3, 2019
- Fixed critical CC3220/CC3120 NWP Issue which resulted in error and halt of execution, where the error state was persistent across device reset. This issue required a use case where the fast connect feature is enabled on the affected devices, and the AP that the device is connected to has at least two of the following authentication modes enabled: WPA2/PSK, WPA2/EAP, WPA2/FT using PSK (802.11r fast transition/fast roaming)