选择版本

选择版本

未找到结果。请清除搜索,并重试。

PROCESSOR-SDK-LINUX-RT-AM65X

适用于 AM65x 的 Linux-RT 处理器 SDK

选择版本
未找到结果。请清除搜索,并重试。
版本: 06.00.00.07
发布日期: 06 七月 2019

Code Composer Studio IDE for Windows Host

Code Composer Studio IDE for Linux Host

AM65x Pin Mux Configuration Utility

Only used when creating an SD Card on Windows

MD5 校验和

Standalone ARM Toolchain - ARM GCC 8.3 2019.03 toolchain

AM65x Linux SDK prebuilt BSP binaries and root filesystem

MD5 校验和

AM65x Linux SDK Arago source downloads

MD5 校验和

Quick Start Guide that was included in the EVM kit

Quick Start Guide that was included in the EVM kit

产品
基于 Arm 的处理器
AM6526 具有千兆位 PRU-ICSS 的双核 Arm® Cortex®-A53 和双核 Arm Cortex-R5F Sitara™ 处理器 AM6528 Sitara 处理器:双核 Arm Cortex-A53 和双核 Arm Cortex-R5F、千兆位 PRU-ICSS、3D 图形 AM6546 具有千兆位 PRU-ICSS 的四核 Arm® Cortex®-A53 和双核 Arm Cortex-R5F Sitara™ 处理器 AM6548 具有千兆位 PRU-ICSS 和 3D 图形的四核 Arm® Cortex®-A53 和双核 Arm Cortex-R5F Sitara™ 处理器

文档

Instructions for creating an SD Card with Linux

Instructions for creating an SD Card with Windows

Link to Release Notes for Processor SDK Linux

Link to the online Software Developers Guide which has the latest content

Software Manifest of Components Inside the SDK

发布信息

Thank you for your interest in the AM65x Software Development Kit (SDK). If you would like to install the full SDK on a Linux Host computer for development, you'll need the AM65x Linux SDK Essentials below. If you would like to evaluate the SDK by running it on one of the below platforms and you prefer not to install the full SDK at this time, please see the AM65x Linux SDK SD Card Creation section below. This SDK supports both AM65x and DRA80xM device families based on code reuse for Arm Cortex-A53 cores.

More Information If you'd like more information on all of these choices, please refer to the Processor SDK Linux Getting Started Guide (GSG) below or the latest version here . For a complete overview of the SDK, please refer to the Processor SDK Linux Software Developer's Guide (SDG) below or the latest version here .