ZHCSQQ4C November 2011 – June 2022 TPA2015D1
PRODUCTION DATA
The TPA2015D1 internal boost converter operates in a discontinuous mode to improve the efficiency at light loads. The boost converter has overvoltage protection that disables the boost converter if the output voltage exceeds 5.8 V. If current is forced into the PVOUT terminal, the voltage clamp will sink up to 10 mA. If more than 10 mA is forced into PVOUT, then the PVOUT voltage will increase. Refer to the Section 9.3.6 section for details.
See Section 13.1.1.2 for a list of terms and definitions used in the boost equations.