ZHCSP44D October 2021 – October 2024 DLP160CP
PRODUCTION DATA
Operational DMD temperature and landed duty cycle interact to affect the usable life of the DMD, and this interaction can be exploited to reduce the impact that an asymmetrical landed duty cycle has on the usable life of the DMD. The relationship between temperature and landed duty cycle is quantified in the derating curve shown in Figure 5-1. The importance of this curve is that:
In practice, this curve specifies the maximum operating DMD temperature that the DMD should be operated at for a given long-term average landed duty cycle.